Part Number: SN54LVTH244A-SP The datasheet does not provide any package information for the 5962-9584401V2A (the LCCC version of this device). The link in the "Ordering & Quality" section of the landing page does not provide any information either.…
Part Number: SN54LVTH244A-SP Does the CDP (W) package for the SN54LVTH244A-SP have a metal lid? and is this lid floating or electrically connected to anything?
The package drawing on the data sheet has a note that says the lid can be ceramic but I saw…
Part Number: SN54LVTH244A-SP Team,
What is the difference between the two OPNs marked in color below? Which one is supposed to be the "flight" part?
https://www.ti.com/product/SN54LVTH244A-SP#order-quality
Thanks in advance,
A.
Part Number: SN54LVTH244A-SP Other Parts Discussed in Thread: SN74LVTH244A Hi Team, Do we have a spice model available for SN54LVTH244A-SP? Kind Regards, Jejomar
Part Number: SN54LVTH244A-SP Could you let me know the package information as follows?
P/N: 5962-9584401VSA
・Package material/ base plating /plating (ex. Ceramic(Alumina)/Ni/Au
・Lid material/ base plating /plating (ex. Covar/Ni/Au
・Package cavity wall…
Part Number: SN54LVTH244A-SPsn54lvth244a-sp data sheet page 7 notes mentions test condition for input transition time to be less than 2.5 nsec.
C. All input pulses are supplied by generators having the following characteristics: PRR ≤ 10 MHz, Z O …
Part Number: SN54LVTH244A-SP Team,
Quick question from my customer:
The data sheet for the 54LVTH244A has the following requirements under recommended operation for power supply rise time:
What is the impact to part functionality if the power system…
Part Number: SN54LVTH244A-SP Are SN54LVTH244A-SP inputs cold sparable? That is .. is there a high side ESD clamp diode? If power is OFF on this device .. and the input is driven from a powered ON device .. will this high side ESD clamp diode form a sneak…
Part Number: SN54LVTH244A-SP Other Parts Discussed in Thread: SN54LVTH244A , SN74LVTH244A Hi Sir/Mdm,
The datasheet for SN54LVTH244A does not indicate any value for IOFF. Is it because it is not tested or there is no such parameter?
Similar part (SN74LVTH244A…
An isolator like the ISO7041-Q1 makes sense only for galvanic isolation.
The SN3257-Q1 would be able to disconnect the signals. Alternatively, use any buffer with Ioff protection, e.g., SN74LV125A-Q1 or SN54LVTH244A-SP.