Part Number: SN54SC8T541-SEP Hi Team,
Could you please help me with designing a circuit using the SN54SC8T541-SEP?
I have one SDA line and one SCL line from an I²C interface. Can I use one SN54SC8T541-SEP to expand the single SDA line into eight SDA…
Part Number: SN54SC8T541-SEP Hi , The is an octal push-pull buffer. The datasheet states: Continuous output current (VO = 0 to VCC ) = ±25 mA Continuous output current through (VCC or GND) ±50 mA IO Output Current (VCC = 4.5V to 5.5V ) = ±25 mA There…
Part Number: SN54SC8T541-SEP For the SN54SC8T541-SEP, can the device inputs be driven (within normal operation per the data sheet) while VCC = 0V? This would be a cold-spare application where one device is powered and the other is not.
Regards,
Rick…
Part Number: SN54SC8T541-SEP Tool/software:
This request is on behalf of my client, Spacemicro/Voyager Space. Wanted to see if there was an ibis model available for the part listed below. Simulating general signal integrity for a board that will be…
Part Number: SN54SC8T541-SEP Other Parts Discussed in Thread: TPS7H4003-SEP
Tool/software:
Hi,
I am attempting to design converting a 2.5V Single Ended clock to 5V using SN54SC8T541-SEP (PN54SC8T541MPWTSEP) for CLK SYNCs to the TPS7H4003-SEP Regulator…
Part Number: SN54SC8T541-SEP Tool/software: Hi,
I couldn't find it explicitly stated in the documentation, so I wanted to verify that:
1) Mixed inputs values can be used. For example, 2.5V and 1.8V signals can be input to a part that has VCC as 3…
Part Number: TPS7H4003-SEP Other Parts Discussed in Thread: SN54SC8T541-SEP , Tool/software: Hi,
I am attempting to design converting a 2.5V Single Ended clock to 5V using SN54SC8T541-SEP (PN54SC8T541MPWTSEP) for CLK SYNCs to the TPS7H4003-SEP Regulator…