Part Number: SN55189A Other Parts Discussed in Thread: ALP Tool/software:
ESD sensitivity?
From the website, - ESD sensitivity is shown as 0 kV. Is this still the case if the unit changes to V instead of kV? We need a classification (0A, 0B, 1A…
Part Number: SN55189A Other Parts Discussed in Thread: MC1489A , , SN75C189A Hi,
We are planning to replace MC1489AN with SN55189AJ as MC1489AN is in LTB.
MC1489AN's operating temperature range is 0°C to 70°C and SN55189AJ's operating temperature…
Part Number: SN55189A Hi,
Does the Dissipation Rating Table in the datasheet talks about the maximum power dissipation that the device can withstand or the maximum power consumed by the device? I think it is the max power dissipation allowed for that…
Part Number: SN75189 Other Parts Discussed in Thread: SN55189A Hi team,
Customer is looking for SN74189 with better temperature range (-40 to 80 or higher). Do we have new portfolio available for this request?
Regards,
Brian