Part Number: SN55HVD251 Orderable Part number
SN55HVD251DRJR
The online datasheet only has the SOIC pinout shown. Can you provide the SON pinout?
Thanks!
Russell
Part Number: SN55HVD251 Other Parts Discussed in Thread: TCAN1042H Hello,
I want to use SN55HVD251 in an application where the CAN signals will be bundled in a connector with +25V and GND. This is a high-cycle connector in a very wet/dirty environment…
Other Parts Discussed in Thread: SN55HVD251 Hello,
The datasheet for the SN55HVD251 doesn't say if the thermal pad be tied to ground. My assumption is yes, but I wanted to verify.
Thanks, Jamaal
Other Parts Discussed in Thread: SN55HVD251 , SN65HVD231 , SN65HVD1040 Good afternoon everybody,
We are having some issues with these devices datasheet (SN55HVD251 and SN65HVD231). It is written on them that they are IS011898 compliant. My question…
Other Parts Discussed in Thread: SN55HVD251 , SN65HVD1050 , SN65HVDA1050A-Q1 I have an automotive sensor we designed with SN55HVD251, and I need to improve the EMC/EMI so I can be certain to pass EMC testing.
How much better is the SN65HVD1050 than…
Other Parts Discussed in Thread: SN55HVD251 Hopefully a really simple one...
I'm designing a board using the SN55HVD251 SON8 package.
I assumed I could connect the thermal pad to ground - but I can't find confirmation for that in the datasheet.…
Calum,
the smallest package for the HVD233 is the 3.9mm wide SOIC-8 package.
the smallest package for any CAN XCVR in TI is the 4mm x 4mm SON-8 for the SN55HVD251.
Regards,
Thomas.