Part Number: SN55LVCP22-SP Other Parts Discussed in Thread: SN55LVCP22EVM-CVAL , 1) For an application in which SN55LVCP22-SP‘s EN0/1 and/or SEL0/1 is not needed to be toggled, would you recommend a certain resistor value for pulling the input low/high…
Michael,
1) This data was taken using a clock source for the two 500Mhz tests. The 1000Mbps is using PRBS2^23-1.
It was noted that at DCA-J86100C was used for the data analysis. It was not noted on the statistical BER setting. Typically during this time…