Part Number: SN55LVDS31-SP Other Parts Discussed in Thread: SN55LVDS31 , I'm trying to verify timing on a project with the SN55LVDS31, however Tsko is somewhat ambiguous. I need to know if the channel-to-channel skew is defined only for like-to-like edges…
Part Number: SN55LVDS31-SP I would like to request the following information for SN55LVDS31-SP
1) Junction-to-Case Thermal Resistance (top)
2) Junction-to-Board Thermal Resistance
3) Weight
Thank you in advance.
Steve
Part Number: SN55LVDS31-SP For board level thermal analysis, do I have to add the solder layer thermal resistance to Junction-to-Case (Bottom) Thermal resistance, when thermal pad is soldered to PCB?
Thank you.
Part Number: SN55LVDS31-SP For thermal analysis of SN55LVDS31-sp , we need following information:
· Weight
· Component core material
· Component package material
· Metal lid material
· Metal lid coating
· Surface color of package (other than…
Part Number: SN55LVDS31-SP Hi, Greetings! Our customer wants to have the PCB footprint for 5962-9762101VFA [CFP (W) |16 ]. We have checked the datasheet as well as the .bxl file available unfortunately we are not able to find it. I would appreciate if…
Other Parts Discussed in Thread: SN55LVDS31-SPSN55LVDS31-SP
Could you let me know the package information as follows?
P/N: 5962-9762101VFA
・Package material/ base plating /plating (ex. Ceramic(Alumina)/Ni/Au
・Lid material/ base plating /plating…
Part Number: SN55LVDS31-SP Table 1 of the datasheet appears to have an error, both Enable columns are designated 'G'. I assume the 2nd 'G' column heading should be 'Gbar' to agree with the logic diagram on page 2?
Thanks, Ted
Part Number: SN55LVDS31-SP Other Parts Discussed in Thread: SN55LVDS32-SP In our application the SN55LVDS31-SP and SN55LVDS32-SP are supplied with 3,3V. The absolute maximum rating is 4,0V.
Assuming a failure case were the supply exceeds the maxium…
Other Parts Discussed in Thread: SN55LVDS31-SP , SN65LVDS31 Hello,
In a new project, we'll use SN55LVDS31-SP drivers between FPGA and ADC.
We have two connection options.
One SN55LVDS31-SP loaded by 6 ADC, ie like in LVDS-M connection (with one…
Part Number: SN55LVDS31-SP Other Parts Discussed in Thread: SN55LVDS31 Hello,
Do you know where I can find the following information for the SN55LVDS31 (Flatpack 16) :
- Die Size (mm²)
- Wire Bonding Material
- Wire Bonding Diameter
- Die…