Part Number: SN65472-EP Hi team,
As per the manual, " Characterized for Use up to 300 mA". Is it possible to get 600-mA output current capability if connecting 1Y and 2Y in parallel?
Thanks.
Best Regards,
Cherry
Part Number: SN65472-EP HI,The datasheet says that Characterized for Use up to 300 mA.So, if I connect 1Y and 2Y together, Is it possible to obtain Driving ability up to 600mA?
Part Number: SN65472-EP Hi Team, Our customer is looking for a similar device to the SN65472-EP which can operate up to 105°C. They've noticed on the first page of the datasheet that a custom temperature range for the device (for up to 125°C temperature…
Part Number: SN65472-EP Hi team, Our customer is experiencing voltage measurement in Inputs 1B and 1A of around 1.4V even without supplying voltage in VCC. Already tested all other boards and experiencing the same issues. Also in 2A and 2B there are 1…
Other Parts Discussed in Thread: DRV8803 , TPL7407L , SN65472-EP , ULN2003A , DRV8844 We have an application where a low-side quad driver needs replacement. The existing quad driver goes under PN A2557KLB. We started investigating the ULN2003A and TPL7407L…
Yuriy,
Given the age of the device (50 years) we would not have any sort of extended parametric data of the device outside of the recommended operating range of what is in the datasheet. We do have a similar high-reliability part that has an extended…
I looked at what is available and found the following are probably best candidates: SN65472-EP, SN75472, and SN75477. I gather the 472 and 477 only come in commercial temperature versions. Would you say the SN65472-EP then the most likely candidate? Following…