Part Number: SN65ALS176 Other Parts Discussed in Thread: THVD1500 Hi team,
Could you please kindly help check if our SN65ALS176 can support 1000m transmission with 115kbps?
Thanks,
Brian
Part Number: SN65ALS176 Other Parts Discussed in Thread: THVD1550 Hi Team,
Would like your support for component survey below. It is important to Rockwell for component resiliency and risk assessment.
Supplier
Supplier Part Number…
Part Number: SN65ALS176 Hi team,
My customer is testing our 485 receiver function.
They only connect the VCC to 5V and the GND to ground, other pins all floating as below:
And they find when they test the A and B, they find A - B=3.8V.
Could…
Part Number: SN65ALS176 Other Parts Discussed in Thread: THVD8000 Dear Sir/Madam,
We require technical support for the RS485 termination resistor requirement. We have used SN65ALS176 as RS485 Transceriver.
Below is our circuit diagram.
All FMs …
Part Number: SN65ALS176 Other Parts Discussed in Thread: THVD1550 Hello,
my customer is looking for an IBIS model of the SN65ALS176DR - can you please help with that.
Thank you and best regards, Dirk
Other Parts Discussed in Thread: SN65ALS176 , THVD1505 , THVD1400 Hi everyone,
SN65ALS176 is declared to work properly between 4.75V and 5.25V
If I suplly the transceiver with a power supply of 4.5-5.5V, what kind of malfunction or degradation should…
Hi Hao,
Yes you are correct V.11/X.27 is deprecated and no longer in use, at least X.27, however V.11 published in 1996 still in force. I made the same conclusions by comparing datasheets for SN65HVD21A and SN65ALS176 which is meet the requirements…
Part Number: SN65HVD3088E Other Parts Discussed in Thread: SN65ALS176 , THVD1550 , THVD1500 Hello,
I want to use SN65HVD3088E for a combined RS485 and RS422 application. The data sheet states compliance to TIA-485-A and TIA-422-B, but supports maximally…
This spreadsheet tool makes it easy to look up what the recommended pin to pin capable RS-485 transceivers to replace old TI RS-485 transceivers.
/cfs-file/__key/communityserver-discussions-components-files/138/1777.Recommended-New-RS_2D00_485-parts…