Part Number: SN65C1168 Please tell me about the power consumption of the SN65C1168.
I believe the SN65C1168 has two built-in driver circuits and two built-in receiver circuits.
I'm using separate elements in two locations.
In one location, I'm using…
Part Number: SN65C1168 Tool/software: I am only using 3 of the 4 channels. What should I do with the I/O of the channel I am not using? Should I leave them unconnected? Should I pull them up/down? And what size pull-up/pull-down resistor should I use…
Part Number: SN65C1168 Hi Team
I have 2 questions regarding SN65C1168 and SN65C1168E.
1, What is the deference of ESD protection spec? I'd like to confirm this because we couldn't find "ESD Protection for RS-422 Bus Pins" at the datasheet of SN65C1168…
Part Number: SN65C1168 Tool/software:
Hi
How many watt is required for the power supply Vcc input to make sure the IC can work correctly ?
in our application we are transmited 2Mbps over 100 meter cable.
Thanks!
Part Number: SN65C1168 Other Parts Discussed in Thread: THVD1520 Tool/software: Hi team,
Could you let me know if SN65C1168 is compatible to RS-485?
It is not clearly mentioned on the datasheet.
I've already checked the previous thread , but it…
Part Number: SN65C1168 From the datasheet, I see there are steering diodes in the part that protect against over-voltage transients. I am in an application where the diferential TX and RX lines must survive a 50V, ~300us transient.
If I use a TVS…
Part Number: SN65C1168 Hi teams,
What is the difference between SN75C1168PWR and SN65C1168PWR except for temp range?
Is it possible to replace SN65C1168PWR from SN75C1168PWR?
Best regards,
Shunsuke Yamamoto
Part Number: SN65C1168 Hello Experts,
I have a DSC card stacked in Peripheral interface card (PIC) both having common power supply 5V and GND. The transceiver IC placed in the PIC is powered by this same 5V and the signals are connected to the transceiver…
Part Number: SN65C1168 Dear sir
Dear We got SN65C1168PWR with lot number 2340095MY2 , Could you please help us to check the lot number? which date code could it refer to? thank you very much!
Part Number: SN65C1168 Other Parts Discussed in Thread: THVD2450 Dear team,
Could you recommend the similar solution with SN65C1168 but can support +/-16V input device?
Thanks.
Regards,
Ben