Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: SN65C1168E-SEP Hi,
For this IC, can customer applied input voltage when there is no Vcc?
For example, 5V at input of driver before voltage is applied to Vcc. If this possible, what is the maximum input voltage is allowed, it is the same as…
Part Number: SN65C1168E Other Parts Discussed in Thread: SN65C1167E , Hi Team,
Pins for 1A, 2A, 1B, and 2B are the noninverting and inverting input pins for receiver 1 and receiver 2. The 1Y, 2Y, 1Z, and 2Z are supposed to be the outputs for receiver 1…
Part Number: SN65C1168E Other Parts Discussed in Thread: SN65LBC174A Hi,
SN65C1168EPWR is two line drivers and two line receivers.
Can I use pins 1, 2, 3, and pins 5, 6, 7 as the line driver?
In this way, I have four channels of line drivers to use.
…
Part Number: SN65C1168E
Hello,
I am designing RS485 interface circuit.
I want to find out if the SN65C1168E can be used in a circuit with an RS485 interface.
Termination resistor of RS485 interface circuit is 120ohm X 2.
And VCC of SN65C1168E is 5V.
…
Part Number: SN65C1168E-SEP Hi there, maybe this is a very basic question. Can this device be used for RS-485? Any special considerations in designing as such?
Part Number: SN65C1168E Hi!
I have a problem with the IC: SN65C1168ERGYR . Does thermalpad need to be connected to GND? It's about the package VQFN16. The documentation does not contain this information. www.ti.com/.../sn65c1168e.pdf Thanks!
Part Number: SN65C1168E-SEP I am interested to know the radiation tolerance of the SN65C1168E-SEP, RS-422 transceiver to Single Event Upset (SEU). Your radiation documentation for this part only lists the tolerance to Single Event Latchup (SEL). Our application…
Part Number: SN65C1168E Hi,
1.) The datasheet does not specify how to tie unused inputs. What does TI recommend?
2.) The datasheet states that “If desired, add external fail-safe biasing to ensure ±200 mV on the A-B port when the driver circuit is disabled…
Part Number: SN65C1168E-SEP Other Parts Discussed in Thread: DS34LV86T , DS34LV87T
Hi,
Can SN65C1168E-SEP operate at VCC=3.3V?
If yes, is there any Electrical Characteristics we can refer at this condition?
If no, can SN65C1168E-SEP at VCC=5V be connected…
Part Number: SN65C1168E-SEP Hello Guys,
Good day.
We have a customer wishing to use SN65C1168EMPWSEP on an orbital flight unit. It's clearly designed for spaceflight, but he did not saw the INST-002 testing, or QML info per MIL-PRF-38534. Is there a screened…