Part Number: SN65C3232 Other Parts Discussed in Thread: TRS3223 , TRS3232E Dear Sir/Ms.
My customer reported that they designed SN65C3232PWPR on their machine and needed to short-circuit the TX. The customer's circuit cannot be placed on the forum,…
Part Number: SN65C3232 Hello,
Since Pn. SN65C3232D was discontinued, our customer changed over to SN65C3232DR. According to its data sheet, only change seems to be the PACKAGING. Besides the packaging, is there any specification difference between SN65C3232D…
Part Number: SN65C3232 Built 10 prototypes, and 2 of 10 provide 'garbage' during RS-232 communication at 155200 bps. Charge pump capacitors are 220 nF 25V X5R at 3.3 V supply voltage. Can it be the problem? What are requirements and tolerance for those…
Part Number: SN65C3232 Hi,
My customer is trying to set each capacitor as below and concern about degrade characteristics as compared to specified characteristics.
C1=0.1μF、C2,=C3=C4=0.47μF
Do these capacitances effect to specified characteristics…
Part Number: SN65C3232 Hello,
I have a design with SN65C3232 and I am concerned by ESD protection. There is not external ESD protection in the design. So, I have two questions:
Datasheet of SN65C3232 says that has ±15 kV Using Human-Body Model…
Part Number: SN65C3232 Other Parts Discussed in Thread: TRS202E
Dears:
From datasheet we can see the receiver's input rin is Open, and the output is H.
However, there is no description of Output state when Input is Open.
Pls. give some advice…
Part Number: SN65C3232E Other Parts Discussed in Thread: SN65C3232 Hi team, Could you please help my customer to check the schematic of SN65C3232EPWR , and if there is any EMI issue in the circuit. I think the schematic of SN65C3232EPWR is good, but I…
Hi Harijith,
I can't specifically say that a device won't EOL or continue to be in production for 10 years.
What I can state is that TI has already gone through the design refresh for the MAX3232E meaning that the MAX3232E is now in TI's latest process…
Part Number: MAX3232E Other Parts Discussed in Thread: TRSF3232E , TRS3232E , SN75C3232 , SN65C3232 Hi
We currently use the MAX3232EIDR Transceiver, we are finding it difficult to get hold of these, also the MAX3232EID is not recommended for new designs…