Part Number: SN65CML100 Tool/software: 1. Are the CML outputs (Y and Z) of SN65CML100 internally terminated with 50ohm to VCC?
2. Does cml100.ibs model include the CML output 50ohm termination resistors to VCC?
Thanks.
Part Number: SN65CML100 Hi,
Good Day. What is the junction to board thermal resistance of SN65CML100DGK?
Please advise. Thank you very much.
Best Regards,
Ray Vincent
Part Number: SN65CML100 Hi,
The SN65CML100 datasheet says VOD is as below when terminated to VTT = 1.8V:
We can see that terminating into 50 ohms doubles the VOD voltage swing compared to 25 ohms.
Is it realistic / allowed / permitted to use 100 ohm…
Part Number: SN65CML100
I would like to simulate the SN65CML100 to confirm its operation for my application. The only available model on the TI website is an IBIS file.
Unfortunately, I do not have access to any software that is compatible with IBIS …
Part Number: SN65CML100 Hi
Trying to use SN65CML100 in my design.
Using Lattice FPGA to drive true LVDS signals and need to convert them to HDMI physical layer compatible (CML)
On terminal side Chip which converts from HDMI (TMDS) to TTL logic for…
Part Number: SN65CML100 Hi,
I would like to use SN65CML100 to convert LVPECL to CML as below figure shows. Where should I add the termination resister for LVPECL?
Thanks.
Part Number: SN65CML100 Other Parts Discussed in Thread: SN65LVDS100 Hi there,
We are looking to use SN65CML100 to recover our ac coupled, high speed CML logic (960Mbps) from long cable loss (3m). The eye diagram of the input looks like below, and it…
Part Number: SN65CML100 Other Parts Discussed in Thread: DS10BR150 I would like to use this part to drive 1.2V CML line. Based on the data sheet and app note, i plan on using two 50 Ohm resistors as bias generators at the output of the chip, connected…