Part Number: SN65DSI84 Other Parts Discussed in Thread: DSI-TUNER Hi Zach,
Since we talked, I didn't fix my issue
We recieved a new board with a new layout, it sould be better than the previous one.
However, with our last configuration I couldn't…
Part Number: SN65DSI84 Other Parts Discussed in Thread: DSI-TUNER Hi
The customer wants to connect the SN65DSI84 through the MIPI DSI interface of the system to convert the LVDS signal >> LCM (support 1920*1080) I would like to ask, if possible …
Part Number: SN65DSI84 Other Parts Discussed in Thread: DSI-TUNER Hi Ti Support team,
I am using sn65dsi84 on nxp i.MX8m mini SOC with yocto platform, kernel 5.15.52.
There has ti-sn65dsi83.c driver in <kernel_root>/driver/gpu/drm/bridge which compatible…
Part Number: SN65DSI84-Q1
Hi ,
Could you help generate a dsi84 test pattern register setting?
LVDS:
1920 x 1080
dual lvds
24bpp
dsi blank:
hfp 64 vfp 70
hbp 32 vbp 8
hpw 32 vpw 8
Single lvds clk 71.6M
de polarity: positive,hs vs polarity: negat…
Hello Zach,
Effectively, we are outside, we try to reduce or disable the spread spectrum.
However, on internal test pattern, we didn't see flickering. If we don't see flickering on internal test pattern, we sould don't see flikcering on normal mode…
Part Number: SN65DSI84 Hello,
We are using the HDA1010WHPT-I-3GHI display along with SN65DSI84
Our DSI CLK is about 222.2MHz.
And using DSI Tuner we have configured following parameters. Are these configurations correct?
We use the test pattern config…
Part Number: SN65DSI84 Other Parts Discussed in Thread: DSI-TUNER Dear Team,
Please help to provide the SN65DSI84 driver for AMBA CV platform design.
Linux : kernel 5.4 version
thanks a lot
Jimmy