Part Number: SN65DSI84 Hello,
We are using the HDA1010WHPT-I-3GHI display along with SN65DSI84
Our DSI CLK is about 222.2MHz.
And using DSI Tuner we have configured following parameters. Are these configurations correct?
We use the test pattern config…
Part Number: SN65DSI84 Other Parts Discussed in Thread: DSI-TUNER Dear Team,
Please help to provide the SN65DSI84 driver for AMBA CV platform design.
Linux : kernel 5.4 version
thanks a lot
Jimmy
Part Number: SN65DSI84 Hi team,
my customer requested below question, could you help?
Can you kindly support on SN65DSI84 part with below query
Can we adjust the drive strength of LVDS ouput signals . is it the CSR register ?
Can we adjust drive strength…
Part Number: SN65DSI84 the correct rating is 2KV (HBM).
I find same question in E2E,it seems to be a typo.
Please send me the correct datasheet of SN65DSI84.
Thanks a lot.
Part Number: SN65DSI84 Dear Team,
We are using SN64DSI84 in our project and bringing up the LVDS panel right now.
Currently REFCLK is DSI clock(495MHz), and expected LVDS clock is 72MHz.
As data sheet mentioned, should keep REFCLK_MULTIPLIER to 0 while…
Part Number: SN65DSI84-Q1 Hello TI experts,
my customer wants to use SN65DSI84-Q1 as single-link LVDS.
LCD module has 1280x480(RGB) resolution and LVDS24(8x3) bits VESA interface.
1. About firmware, we will set LVDS_LINK_CFG as 1, to set single-link LVDS…