Part Number: SN65DSI86-Q1 Other Parts Discussed in Thread: SN65DSI86 Hi, TI.
I have a problem that the color tone is different between the input and the output.
When using Color bar pattern in 0x3C, work good.
Is there a setting or mode to swap RGB?
Are…
Part Number: SN65DSI86-Q1 Hi Brian,
For SN65DSI86-Q1 HPD pin voltage, the datasheet recommend min threshold 2.2V @51k ohm, but no max value displayed. Does that means no max limits?
If increase 2.2V to 5V, should we increase external resistor value to…
Part Number: SN65DSI86-Q1 Other Parts Discussed in Thread: SN65DSI86 , TDP142 Is there a EVM of the TQFP based SN65DSI86 device, can you please share the PCB files for the corresponding EVM? Thank You.
Part Number: SN65DSI86-Q1 Hi Team,
Customer is using SN65DSI86-Q1 for 4k bridge, but they find the SOC can output 1080 x 3840 only. So they wonder if SN65DSI86-Q1 can covert 1080 x 3840 to 3840 x 1080?
If can't, customer may have to add one chip to do that…
Part Number: SN65DSI86-Q1 Other Parts Discussed in Thread: SN65DSI86 Hi Team,
Customer found when back-end port performs hot plug quickly several times, the SN65DSI86 shows error and can’t process HPD interrupts normally.
Do SN65DSI86 support quick…
Part Number: SN65DSI86-Q1 Hi Team,
May I know if any indication registers in SN65DSI86-Q1 which can monitor MIPI input data is correct data or not?
Best Regards, KL
Part Number: SN65DSI86-Q1 Other Parts Discussed in Thread: SN65DSI86 , TEST2 Hi, TI.
I use SN65DSI86 in MIPI DSI receiver, and TC358778(TOSHIBA) in RGB-DSI converter. My system has the TC358778 receiving RGB data and passing it to the SN65DSI86 using the…
Part Number: SN65DSI86-Q1 Other Parts Discussed in Thread: SN65DSI86 , TEST2
Hi team,
I was Implemented GPU software to read the panel EDID information and program the DSI86 Video Registers with the Video format that is expected to be displayed on the…