Part Number: SN65HVD10 Team, am I misreading figures 18 and 19 for VOH and VOL vs. load current?
I think 18 is measuring V OA and 19 is V OB ?
1) If true how why do the figures have negative voltage?
2) Since V CC is 3.3V why does the x-axis go…
Hi Dattatray,
As I said above, the simplest solution is likely to only include the fail-safe circuit on a single node. If it is guaranteed that this system will always have one and only one master node, the circuit can be included here and on none of…
Part Number: SN65HVD10 I have a question regarding input protection on the SN65HVD10D opamp. We experienced an event where the input voltage (D and DE) was 32V for an unknown, but short amount of time. This opamp was powered by a power supply with a 1A…
Part Number: SN65HVD10 Hi Sir
my customer is use 3.3V in MCU and SN65HVD10, the customer question if output A/B need connect to pull high resistor?(they don't understand how A/B pin voltage can reach 12V)
May we have reference circuit? i see datasheet…
Part Number: SN65HVD10 Hi, could anyone help me with decoding date codes to determine when the parts were produced?
marking is VP10Q which is SN65HVD10QD
remaining markings:
part 1: 4CM A7HE
part 2: 59M AHE1
Thank you!
Part Number: SN65HVD10
Hi TI Support Team,
Can you please help with below concern?
We have SN65HVD10D/RS485 Modbus Interface in our system.
Line Voltage Fan with Modbus
VFD (Motor Drive) with Modbus
Control Board with Modbus
Hence, each…
Kay,
Do you mean SN65HVD10 and MAX3221 share a same wire? It's OK to do so, but please be aware that SN65HVD10 bus pins have -9V to 14V abs max. Theoretically RS-232 signal swing from -15V to 15V. However MAX3221 Dout range is much smaller than that…
Part Number: SN65HVD10 Hello,
Is there a finite period of time that the output can sustain a short circuit to ground? If so what is the criteria? The data sheet shows there is short circuit protection but does not specify if it is indefinite. Due…
Part Number: SN65HVD10 Hi
My customer is requesting for low propagation half-duplex RS485 solution. For SN65HVD10, driving propagation delay is MIN/MAX 5ns/16ns, receiving propagation delay is MIN/MAX 12.5ns/25ns. Customer need MAX-MIN is less than…