Part Number: SN65HVD1050 Hi,
My customer has a question regarding the max and min signaling rate limitation of CAN bus transceiver.
For example, the recommended signaling rate for SN65HVD1050 is 20kbps to 1Mbps. Actually my customer is curious why there…
Part Number: SN65HVD1050
Hi,
The customer has been using SN65HVD1050 for a long time and found that the voltage on the Bus side was overshooting. Do you know the cause of the overshoot? I attached the material, so please refer to the circuit diagram and…
Part Number: SN65HVD1050 Hi Team, our customer is asking SN65HVD1050 support CAN2.0. because their requirement is "All CAN bus transceivers SHALL support CAN2.0"
Thank you in advance
Part Number: SN65HVD1050 Hi team,
Could you kindly advise the Icc in the below conditions?
<Customer’s conditions>
- Node 30
- Termination 120 ohm (both end of the bus)
<Questions>
- Is the Icc of receiver node same with the Icc…
Part Number: SN65HVD1050 What are the requirements for the routing of SN65HVD1050 CAN communications?
Whether need to take the differential line? What is the wire diameter of the line? How much pitch between CANH and CANL is appropriate?
How many ohms o…
Part Number: SN65HVD1050 Other Parts Discussed in Thread: STRIKE , TCAN1051 dear Sir,
my customer used SN65HVD1050, it is failed return back from end customer, we find fin7 (CAN_H) short to the Ground.
there are happened three times for this issue.
below…
Part Number: SN65HVD1050-EP Other Parts Discussed in Thread: SN65HVDA1050A-Q1 , SN65HVD1050-Q1 Hi Team,
Related to the question in the other thread:
In the datasheet, it is stated that it withstands voltage transients from –200 V to 200 V, according to…
Part Number: SN65HVD1050 Other Parts Discussed in Thread: TCAN1051-Q1 , TCAN1051V-Q1 , TCAN1042-Q1 What would happen if the Vref pin (pin 5) of SN65HVD1050 were to be back-driven by 3.3V? Since the functional block diagram doesn’t really indicate what the…