Part Number: SN65HVD1050 Other Parts Discussed in Thread: , , TCAN1051 Please can someone tell me what the differences are between the three CAN transceivers sn65hvd1050, sn65hvd1050a-q1 and sn65hvd1050-q1. Basically our supply chain department has inadvertently…
Other Parts Discussed in Thread: SN65HVD1050 , SN65HVDA1040A-Q1 , SN65HVD1050-Q1 , SN65HVDA541-Q1 , SN65HVDA540-Q1 Hi
I am using the sn65hvd1050 CAN transreceiver for CAN interface . When I give the logic high to strobe pin(8) of transreceiver it not…
Part Number: SN65HVD1050-EP Other Parts Discussed in Thread: SN65HVDA1050A-Q1 , SN65HVD1050-Q1 Hi Team,
Related to the question in the other thread:
In the datasheet, it is stated that it withstands voltage transients from –200 V to 200 V, according to…
Part Number: SN65HVD1050
Hi,
The customer has been using SN65HVD1050 for a long time and found that the voltage on the Bus side was overshooting. Do you know the cause of the overshoot? I attached the material, so please refer to the circuit diagram and…
Part Number: SN65HVD1050 Other Parts Discussed in Thread: TCAN1042V-Q1 Dear,
our client use TJA1049T, and we find SN65HVD1050 maybe can replace, but we saw the SN65HVD1050 cannot support standby mode and data rates up 1M.
have other suggestion, Please advise…
Part Number: SN65HVD1050 Other Parts Discussed in Thread: TCAN1051-Q1 , TCAN1051V-Q1 , TCAN1042-Q1 What would happen if the Vref pin (pin 5) of SN65HVD1050 were to be back-driven by 3.3V? Since the functional block diagram doesn’t really indicate what the…
Hi Eric,
I had not made the link between the Q1 suffix and ISO7637, also because the SN65HVD1050 (without Q1) datasheet does mention ISO7637.
We design and sell autonomous energy systems, using 12V, 24V and 48V batteries. We have had failures of the SN65HVD1050…
Part Number: TCAN1042-Q1 Other Parts Discussed in Thread: SN65HVD1050-Q1 Can we use TCAN1042-Q1, when we use SFA J1939 plotocol?
SN65HVD1050-Q1 datasheet was wrote "SAE J2284 High-Speed CAN for Automotive Applications". However, TCAN1042-Q1 datasheet…
Part Number: SN65HVD1050 Other Parts Discussed in Thread: TCAN1051-Q1
my customer is using SN65HVD1050DR for the BLDC Driving Board and found when the board just power on, the IC temp will rise to 50c degree very soon which even hotter than the power…
Other Parts Discussed in Thread: SN65HVD1050 , SN65HVDA540-Q1 , CD4055B , CD4066B-Q1 Hello,
Are there any switching device or Application for switching CAN - RS232? Please see the attached picture. I serarched digital logic device, mux device in website, but…