Other Parts Discussed in Thread: SN65HVD11 Hi,
Are there any problems with the use of SN65HVD11 in an environment that is directly exposed to the nitrogen gas?
Package Type : SOIC Lead/Ball Finish : CU NIPDAU
Best regards, Seishin
Hello Brian,
According to the Part Marking Lookup on ti.com, a VP11 is a :
SN65HVD11D VP11 D | 8 ACTIVE 3.3V Differential Transceiver
SN65HVD11DG4 VP11 D | 8 ACTIVE 3.3V Differential Transceiver
SN65HVD11DR VP11 D | 8 ACTIVE 3.3V Differential Transceiver…
Other Parts Discussed in Thread: SN65HVD11 hello,
How do we calculate the power consumption of a SN65HVD11 RS-485 (data converter chip), is there any information in the datasheet?
Thanks.
Other Parts Discussed in Thread: TPS76901-HT , TMS470R1B1M , SN65HVD11-HT Dear Sir/Madam I want you to find some type of high temperature chips show as below: TMS470R1B1M; SN65HVD11-HT; TPS76901-HT ; SM28VLT32-HTbecause I can't find any exact model/type…
Part Number: ISO1410DWEVM Other Parts Discussed in Thread: SN65HVD11-HT I need a high temperature package with robustness similar to ISO1410DW. Tolerance to sustained temperatures above 250C will be necessary. Does this exist?
Hello Vladimir,
Sorry for the delay on this, the reason of why it ’ s not working is because the DTR (active low) signal transceiver on the example (page 12 ) is denied (DTR_n) and the transceiver that you are using (SN65HVD11 ) this signal is “active…
Hi Eric,
A bit more information about your RS-485 network would be useful in determining the appropriate transceiver to use. Specifications such as bus length, number of nodes, and data rate would be useful in narrowing down the possibilities. Do you…
Other Parts Discussed in Thread: OPA211-HT , INA333-HT , SM28VLT32-HT , REF5025-HT , ADS1282-HT , ADS8320-HT , SN65HVD11-HT , SN65HVD1040-HT Hi,
I am looking for eagle library's for some of high temperature components from Texas. Can anyone suggest…
Currently, the customer is having issues establishing a robust system on surface using the SN65LBC176A-EP. Once they are confident that the system is robust and working the way they want, they will be implementing it in a high temperature application…