Part Number: SN65HVD1476 Is it possible to configure RS485 in a multi-master setup with full-duplex communication using the SN65HVD1476?
If so, How do I configuration it?
Part Number: SN65HVD1476 There is an app note (AN-805) that explains how to calculate power dissipation for a differential line driver, but is there anything that can explain the receiver portion?
Part Number: THVD1452 Other Parts Discussed in Thread: SN65HVD1476 , , SN65HVD76 , SN65HVD1473 , SN65HVD73 Hi Team,
My customer wants to know if there is any notes among RS485 drivers, THVD1452, SN65HVD1476 and SN65HVD76. As far as I checked, it looks…
Part Number: SN65HVD1476 Figure 29 of the SLLSEJ8D version of the datasheet appears to indicate that the output impedance of the driver stage (Y & Z) would be high even when the device is unpowered. The ABS max ratings suggest this would be true for voltages…
Part Number: THVD1552 Other Parts Discussed in Thread: SN65HVD1476 , THVD1452 I'd like to implement a full duplex RS-482 bus. I'm thinking about using THVD1552 for the master and SN65HVD1476 for all slaves. I cannot use SN65HVD1476 for the master because…
Part Number: SN65HVD3086E Other Parts Discussed in Thread: SN65HVD1476 , SN65HVD34 Hi
C8051F384 with RS422 - 4 wire Full duplex communication ,
In the F/W Development
What is the Difference Half Duplex and Full Duplex in coding
Is standard keil…
Part Number: SN65HVD71 Other Parts Discussed in Thread: SN65HVD1471 , SN65HVD1470 , SN65HVD70 , , SN65HVD73 , SN65HVD1473 , SN65HVD74 , SN65HVD1474 , SN65HVD1476 , SN65HVD76 , SN65HVD77 , SN65HVD1477 I can see that the ESD levels are higher and the thermal…
Other Parts Discussed in Thread: SN65HVD1476 Hi
I am finding a typical issue in the SN65HVD1476 IC. I am able to receive the data on Rx+ and Rx- line.
But same time, during transmission the data send is not observed on Tx+ and Tx- line.
Subrat,
The internal SCI boot-loader does not have such a support. When you say "RS-485", are you talking about a "true" RS-485 bus with multiple nodes? Or are you talking about a point-to-point network with two nodes, but needing balanced differential…