Part Number: SN65HVD1781-Q1 Other Parts Discussed in Thread: SN65HVD1781A-Q1 , What is(are) the difference(s) between SN65HVD1781-Q1 and SN65HVD1781A-Q1 ?
Regarding SN65HVD1781-Q1 ("A" version DS is the same):
What is the max. |Vod| for 4.75V <= Vcc…
Part Number: SN65HVD1781
Hi Ti,
I bulit two pieces of SN65HVD1781D in my FPGA board, the schematic is as below, I am trying send text data from NB through USB to RS485 cable to SN65HVD1781D in the FPGA board, it looks like that the SN65HVD1781D can…
Part Number: ISO7762-Q1 Other Parts Discussed in Thread: SN65HVD1781 , Hello, As per the specification of SN65HVD1781 , the receiver output high-level voltage (VOH) is specified as 2.4 V to (VCC – 0.3 V) .
For a 5 V supply, this corresponds to a maximum…
Part Number: SN65HVD1781 Tool/software: Hi Team,
I'm planning to use the SN65HVD1781D in one of my 3.3V systems. While reviewing the datasheet, I noticed that under the Features section, it mentions support for 3.3V or 5V systems . However, in the Pin…
Part Number: SN65HVD1781-Q1 Other Parts Discussed in Thread: ESDS552 Tool/software: Hi Team,
We are currently operating our RS-485 bus at 3.3 V and would like to clarify the following regarding the reserved, unpopulated pull-up and pull-down resistors…
Part Number: SN65HVD1781-Q1 Tool/software: Dear TI experts,
My customer failed EMC CE current test of their product using SN65HVD1781-Q1.
1) Average and peak values are exceeded in measuring CE Current in 80~90MHz bandwidth.
2) Max exceeded value…