Part Number: SN65HVD1782-Q1 Other Parts Discussed in Thread: SN65HVD10 Hello team,
Three inputs for SPI communication are required, so "one line driver receiver" and "two line receivers" will be implemented. Is it common to use multiple…
Part Number: SN65HVD1782 Tool/software: WEBENCH® Design Tools Dear Sir,
Sir we are using SN65HVD 1782 IC for Rs 485 communication with my controller.we have total 40 nodes linked in a daisy chain to each other at a length of about 25 meter.
sometimes…
Part Number: SN65HVD1782 Hi,
I'm currently using part SN65HVD1782 for RS485.
Can you tell me if this interface will support J1708 protocol.
If it does support J1708, is there much of difference to the driver circuit?
Regards,
Liam
Part Number: SN65HVD1782-Q1 Hi, team,
My customer used SN65HVD1782-Q1 in system, when doing power switch test, VCC power will restart when VCC has not dropped to 0V, at around ~1V.
Could you please check what is the POR for this device? Thus we can judge…
Part Number: SN65HVD1782 Other Parts Discussed in Thread: TMUX1119 Tool/software: WEBENCH® Design Tools Hi
Greeting for the day
I want to use Sn65hvd1782 for my applcation to convet my signal to Rs485. But the problem is that i have only One enabling…
Part Number: SN65HVD1782-Q1 Other Parts Discussed in Thread: THVD2450 , SN65HVD1782 ,
Dear team,
1. What is the parasitic capacitance requirement for TVS devices when RS485 is operating at 10MHz? Less than 10pF? 20pF?
2. What are the function of R1 and…
Part Number: SN65HVD1782-Q1 Hello,
Can you tell me if the SN65HVD1782-Q1 a bipolar, BiCMOS or a CMOS device?
I am considering using the SN65HVD1782-Q1 in a CubeSat and radiaiton effects depends on the technology used.
Thank you
Part Number: SN65HVD1782-Q1 We are using the device SN65HVD1782QDRQ1 to interface 5V power supplied devices, which require a VIHmin of 0.7xVCC = 3.5V. The datasheet of SN65HVD1782QDRQ1 ( www.ti.com/.../sn65hvd1781-q1.pdf )mentions in Page5, that…
Part Number: SN65HVD1782 Other Parts Discussed in Thread: SN75176B , , SN65HVD75 Hello
My customer see in SN75176B data sheet that
"input impedance ri=12kohm (MIN) ".
However, customer don't find imput impedance spec. in SN65HVD75 and SN65HVD1782…
Part Number: SN65HVD1782-Q1 Hello,
In the SN65HVD1782-Q1 datasheet MIN and TYP |VOD| are not provided for a load of 100 Ohm, a VCC of 3.3V and a temperature of 85C. Can you give me those values?
Thank you
Francesco