Part Number: SN65HVD1782-Q1 Hi, We are performing worst case analysis. There are some doubts regarding the SN65HVD1782-Q1 specifications. 1. The levels VOD, VOC(SS) is marked in the below diagram as per our understanding. Is our understanding correct? Does…
Part Number: SN65HVD1782-Q1 Hello,
I had a followup question:
I see the maximum allowable part height in the drawing, but not a reference for the minimum. As has come up in our other vendor conversations, if TI can provide any information about the minimum…
Part Number: SN65HVD1782-Q1 Hello,
My customer is looking for information about package dimensional tolerances and the maximum pressure or compressive forces that can be applied to the top of the packages for possible top cooling/heat sink applications…
Part Number: SN65HVD1782-Q1 Hello:
The customer is currently using a TI chip SN65HVD1782QDRQ1, which fails after power on. They use two chips to convert clock signal CLK and data signal SIMO of SPI signal into differential signal output. The schematic…
Part Number: SN65HVD1782-Q1
Hi,
Customer want to know if we have data for the current consumption of RS485 and RS422 (100 ohm load) at 10Mbps that we can provide to them. Or If there is a graph that extend up to 10Mbps with 54 ohm load and 100 ohm load. Will…
Hi Sean,
We don't have an IBIS model for this device. Can you use a similar device to test the signal integrity analysis on?
https://www.ti.com/product/SN65HVD1782-Q1#design-tools-simulation
^This device covers the same data rate so it should be a…
Part Number: SN65HVD1782-Q1 Other Parts Discussed in Thread: SN65HVD10 Hello team,
Three inputs for SPI communication are required, so "one line driver receiver" and "two line receivers" will be implemented. Is it common to use multiple…
Part Number: SN65HVD1782-Q1 Hi, team,
My customer used SN65HVD1782-Q1 in system, when doing power switch test, VCC power will restart when VCC has not dropped to 0V, at around ~1V.
Could you please check what is the POR for this device? Thus we can judge…
Part Number: SN65HVD1782-Q1 Other Parts Discussed in Thread: THVD2450 , SN65HVD1782 ,
Dear team,
1. What is the parasitic capacitance requirement for TVS devices when RS485 is operating at 10MHz? Less than 10pF? 20pF?
2. What are the function of R1 and…
Part Number: SN65HVD1782-Q1 Hello,
Can you tell me if the SN65HVD1782-Q1 a bipolar, BiCMOS or a CMOS device?
I am considering using the SN65HVD1782-Q1 in a CubeSat and radiaiton effects depends on the technology used.
Thank you