Part Number: SN65HVD1792 Hi there,
My customer supplies 5V to the Vcc of HVD1792 but would like to know if the I/O pins can work at 3.3V voltage level.
From the datasheet, the min. of VIH is 2V so I guess it might work at 3.3V?
Best regards,
Roy Hsu …
Can I take the common-mode range specification to mean that the device will fully function without performance or reliability degradation if the the device is used on 2 boards with power supplies that are +25V apart?
Other Parts Discussed in Thread: SN65HVD1786 , SN65HVD1792 We are using SN65HVD1792 and SN65HVD1786 RS-485 transceiver chips, and I need to find out if they are fully RS-485 compliant, and if not, in what way(s) they are not.
Some TI datasheets specify…
Hello, guys,
I came up with the same doubt because of the table "ABSOLUTE MAXIMUM RATINGS" on the datasheet (SLLS872H) that shows the maximum ratings for the A & B pins, but not for the Y & Z for that part (not explicitly).
Maybe it would…
Hi Koteshwar,
Thank you for your reply.
In addition, please confirm that there is no problem with the difference in supply voltage for the built-in failsafe circuit of ISO1432 and the
failsafe function of SN65HVD1792 to be used by the communication partner…
Other Parts Discussed in Thread: SN65HVD1792 Team,
Extreme Networks was told by someone at TI that the SN65HVD1792 will operate at 3.3V even thought the datasheet states 5V . They were told that the HVD1792 device will meet the datasheet specs of the HVD1781…
Other Parts Discussed in Thread: SN65HVD73 , SN65HVD1792 I'm looking at using the SN65HVD73 transceiver in a new design primarily because of the I/O protection and increased receiver hysteresis values. The problem is I am required to use a 5V supply…
Other Parts Discussed in Thread: SN65HVD1792 , SN75ALS171A , SN65HVD82 Hi All,
I have an industrial project where there will be one master controller connected to six (6) slave controllers. The physical location of the plant is such that it would be very…
Other Parts Discussed in Thread: SN65HVD1792 Hi
I use rs485 to communicate between PC and cc1110. I use SN65HVD1792 transciever to run rs485 bus on CC1110 side. AS the transceiver needs control on DE and ~RE, I am thinking to use TR and CT of CC1110 as…
This spreadsheet tool makes it easy to look up what the recommended pin to pin capable RS-485 transceivers to replace old TI RS-485 transceivers.
/cfs-file/__key/communityserver-discussions-components-files/138/1777.Recommended-New-RS_2D00_485-parts-for…