Part Number: SN65HVD1793 Other Parts Discussed in Thread: THVD2450 , SN65HVD37 My customer is looking at Full Duplex RS422 with 10Mbps in Motor Motion Control application. The most important parameter for system is Hysteresis voltage (VHYS). I don't see…
Part Number: SN65HVD1793 Hi team,
Is SN65HVD1793 RE internally pulled up?
Is DE internally pulled down?
If it is pulled, could you please specify the pull up/down resistance respectively?
Also, does D pin have internal pull-up or down as well?
Regards…
Part Number: SN65HVD1793 Other Parts Discussed in Thread: ISO1412 What is the best isolated RS-422 part for the following requirements:
- Full duplex
- Speed 500kbps - 20Mbps
- Isolation voltage doesn't matter
I am interested in parts with and without…
Part Number: SN65HVD1793 Hi team,
When fix DE(pin#4) to High with pull-up and RE(pin#3) to Low with pull-down, could you please tell us what the recommended pull-up resistor for DE and pull-down resistor for RE are, respectively? (Vcc=5V)
Regards,
Jun
Hi Barry, the SN55LBC172 is a 10 Mbps device, while the SN65HVD10 supports up to 32Mbps with very short rise and fall times. Your customer's EIA-485 non-compliant application might include the use of unterminated bus lines. Whatever they spec. discloses…
This spreadsheet tool makes it easy to look up what the recommended pin to pin capable RS-485 transceivers to replace old TI RS-485 transceivers.
/cfs-file/__key/communityserver-discussions-components-files/138/1777.Recommended-New-RS_2D00_485-parts-for…