Part Number: SN65HVD232 Other Parts Discussed in Thread: TXU0202-Q1 , TCAN3403-Q1 Tool/software: Hi Team,
I am using SN65HVD232QDRQ1 in my design. Please review the design and provide feedbacks if any.
Thanks,
Shifali N
Part Number: SN65HVD232 Hi, Im using SN65HVD232 in my design suppled with 3.3V. but the CAN High voltage im is getting 3.6V whereas as per datasheet CANH voltage level is is 2.45 to VCC.
Part Number: SN65HVD232 Other Parts Discussed in Thread: TCAN1057-Q1 Hi Team
Customer legacy project used SN65HVD232 with 5V power rails. They found this device is not for 5V power rail until recently.
But the circuit work well in the past and no…
Part Number: SN65HVD232 Other Parts Discussed in Thread: TCAN3414 , Tool/software: Hi Team,
A few questions regarding the new TCAN3414 as I'm considering moving away from the SN65HVD232.
Is this pinout and functionally compatible with the SN65HVD232…
Part Number: SN65HVD232 Hi team
Customer use SN65hvd232 in the single phase inverter, they find when more than one CAN node attached to the CAN network, the differential voltage of CAN_H and CAN_L has some interfere on it, but if there is only one CAN…
Part Number: SN65HVD232 Hi Experts,
Please advise to the query from Cx:
We are using the SN65HVD232D 3.3-V CANBus Transceiver.
Can you tell me what would happen if pin 8 is connected to ground?
I know the datasheet indicates this pin is no-connect…
Part Number: SN65HVD232 hi, im using SN65HVD232 in my design interfacing with ST32F103C8T6. Some times the ic burns without no reason when connecting to bus. here with i have attached the schematic please check.
Part Number: SN65HVD232 Hello, im using SN65HVD232QDRG4Q1 and we want if it component is compatible with SN65HVD232QDRQ1.
I cant found in the documentation the difference between both and the explain for G4 number.
Thanks
Part Number: SN65HVD232
Hello Team,
My customer has some questions for canbus line. can they add a capacitor to the canbus line?
does it bock out noise on the line?
Regards,
Renan