Part Number: SN65HVD232Q-Q1 Hello,
The customer uses the SN65HVD232Q-Q1 product without an external 120 ohm resistor, and the hidden voltage level of CAN-H and CAN-L is only 1.3V, which is much lower than the 2.3V in the manual. The impedance test is…
Part Number: SN65HVD232Q-Q1
Tool/software:
Hi Experts,
Good day!
I'm looking for the thermal resistance information for the p/n below. No information in the datasheet can you share with us the thermal resistance and theta-JC of the device?
…
Part Number: SN65HVD232Q-Q1 Hello,
We would like to do Bulk current injection test on the CAN communication line.
Before going in to the actual lab test we would like to simulate the bulk current injection in the CAN communication line.
We know…
Part Number: SN65HVD232Q-Q1 I need to use this SN65HVD232Q-Q1 IC for CAN interface and was unable to get the req result. My design gives a noisy waveform of CANH and CANL. The voltages I get are" 1: 3.3V, 2: 0V, 3: 3.3V, 4: 3.3V, 5: 0V, 6: 2.25V, 7: 2…
Hi Amelie,
The SN65HVD23x family comes in -Q1 versions:
http://www.ti.com/product/SN65HVD232Q-Q1
http://www.ti.com/product/SN65HVD233-Q1
Please let us know if you have any questions on these devices.
Regards, Max
Hi Richard, I missed that it has to be a 3V3 device. I have put together a comparison with 3V3 devices here ->
http://www.ti.com/assets/js/compareParts/compare.html?familyId=540&parts=TCAN330,TCAN332,TCAN334,TCAN337,SN65HVD232Q,SN65HVD234-Q1,SN65HVD1040…