Part Number: SN65HVD234-Q1 Other Parts Discussed in Thread: SN65HVD234 I need a reference design to interface SN65HVD234-Q1 CAN Transceiver IC with microcontroller. Please assist for the same.
Part Number: SN65HVD234 Other Parts Discussed in Thread: LAUNCHXL-F28379D Hi,
Good Day. I have a customer who is working with SN65HVD234 and have a query with regards with CAN-bus : Voltage level at CAN_High & CAN_Low.
Please see below his query for…
Part Number: SN65HVD234 Hi
Our system using SN65HVD234D for CAN communication .
But we have some isseus CAN communication.
This is our TEST result
1) System Side SN65HVD234D ( Termination Resister 120ohm ) ==== > CAN Device ( Termination Resister 120o…
Part Number: SN65HVD234 Other Parts Discussed in Thread: SN65HVD257
Hi guys.
I have the CAN transceiver SN65HVD234 on my device (in some application I used SN65HVD257 instead of SN65HVD234).
The two pins CANH and CANL are protected from ESD events with…
Part Number: SN65HVD234 Hi Team,
I would like to know the worst cased value of input capacitance (CANH or CANL) of SN65HVD234. According to data sheet, input capacitance is 40pF as typical value. Is there any tolerance? It means there is MAX value and MIN…
Part Number: SN65HVD234-Q1 Other Parts Discussed in Thread: SN65HVD234 , Hi,
Is it possible to use the SN65HVD234 reference for CAN FD at 1Mbps?
Thanks,
Part Number: SN65HVD234-Q1 Other Parts Discussed in Thread: TCAN334 , SN65HVD234 , TCAN334G Hello,
In our requirement specifications, we have to justify that we meet the following requirements for the can bus IO:
Differential input capacitance < 170pF…
Part Number: SN65HVD234 hi: ti
i have 3 questions ,pls help me
1: Recessive voltage is not stable
when we test the signal CAN-SN65HVD234D ,found that the Recessive voltage is not stabel , pls help to explain it;
see the waveform below;
2: we use CAN…
Part Number: SN65HVD234 Hi team,
Found that a file to explain the Grounding and Isolation for RS485 devices as below, but want to check with you if CAN devices can also share this Grounding info, especially for the ground potential differences?
Thanks…
Part Number: SN65HVD234 Hi Team,
The layout section in the datasheet mentions some passive component on input and output of the IC connections. I understood the use of resistors on RX TX lines to limit current. My doubt is when I am not using this CAN…