Hi Eric:
Also the reading for 8V and 12V were different than the ones provided since they seem like the device was working normal, in our reproduce test they were still following the input voltage as expected not like images provided.
We suspect a setup…
Part Number: SN65HVD235 Other Parts Discussed in Thread: TPS763 , LM5165 Hi team,
one of my customers would like to use a DC/DC switching regulator as power supply for the SN65HVD235.
In the datasheet a LDO (TPS763) is recommended but:
- Is the transceiver…
Part Number: SN65HVD235 Other Parts Discussed in Thread: STRIKE Hi All:
For the CAN transceiver what is the ESD testing profile and what method was used like resistance/capacitance for testing the device.
On a previous version of the datasheet it stated…
hi,
i tried to transmit CAN frame using CAN module in processor.I connect the oscilloscope to the CAN controller TX pin of transceiver and ground pin and transmit CAN frame is observed in scope. But nothing is coming out of the CANH and CANL pins .What…
Other Parts Discussed in Thread: SN65HVD235 Is there a known number or estimate of 15kV HBM ESD shocks that the CAN module can handle before its internal ESD diodes will start to fail?
-Jaden
Other Parts Discussed in Thread: SN65HVD235 The SN65HVD235 datasheet states "Bus-Pin ESD Protection Exceeds 16-kV HBM". Does the Human Body Model (HBM) capture both air-gap discharge and contact discharge? That is, does the SN65HVD235 guarantee protection…
Other Parts Discussed in Thread: SN65HVD232 , SN65HVD235 , CC2520 , MSP430F5438A , SN65HVD255 Hello,
I need to implement the functionality of "sending out a single CAN-Message to other nodes" if a boolean state changes on my PCB.
Overall number…
Hi Jeffrey,
See this thread's suggested answer for a quick explanation of the CAN passive error:
https://e2e.ti.com/support/interface-group/interface/f/interface-forum/727465/sn65hvd235-can-passive-error-flag
The fact that the passive error is happening…
Part Number: TMS320F28377D Other Parts Discussed in Thread: SN65HVD235 Hi all,
I have been trying to set a CAN communication between CANA and CANB based on can_external_transmit.c example
I have no access to the same example PINs for CANbus, namely 30…
Part Number: TCAN1044V Other Parts Discussed in Thread: SN65HVD235 , TCAN1043-Q1 , SN65HVD233 Hi Team,
i have several questions about our TCAN devices, please kindly help to answer. Thanks.
do we have any TCAN devices which can support loopback mode, MCU…