Part Number: SN65HVD230 Other Parts Discussed in Thread: SN65HVD234 , SN65HVD233 , SN65HVD235 Hi Team, Our customer is using the SN65HVD230 for their sensor design. They intend to bring the CANH and CANL from the SN65HVD230 outside the sensor for the user…
Part Number: SN65HVD235
Im facing difficulties on understanding the datasheet of SN65HVD235. I need the propagation delay of the device to use as input for the CAN Bit Timing calculatior (SPRAC35). The calculator uses:
total propagation time = 2 x (delay…
Part Number: SN65HVD23 Hi,
I wanted to know the current required(max current consumption) for the below mentioned parts
SN65HVD233
SN65HVD234
SN65HVD235
Regards,
Karthik
Part Number: TMS320F28377D Other Parts Discussed in Thread: SN65HVD235 Hi,
I tried to start CAN communication from external loopback example. What I did is just modifying GPIO pin which we use (GPIO 5/4), and everything else is kept unchanged. But when…
Hi Hiroyaka-san,
After looking at the DeviceNet spec a second time I realized that the bus fault protection on the TCAN33x devices does not meet the DeviceNet spec. The TCAN33x devices suyport +/-14V while the SN65HVD252/3 devices support -36V to 40V…
Other Parts Discussed in Thread: SN65HVD235 Hai,
I want to inspect/read a CAN bus. In the market I found a lot of CAN analyzers, but the cost is not affordable for me. So I decided to make a simple CAN bus analyzer. I know the basic CAN communication…
Hi,
I aslo have this problem.
I'm using 2 nodes on BUS, the one is Dspic30F4011 used MCP2551(5V) as transceiver and the other is TMS F28335 used SN65HVD235 (3.3V) as transceiver. The problem is, they can't communicate with each other.
Could…
Other Parts Discussed in Thread: SN65HVD235 I am wondering where the RC filter should be put in CAN and RS485 networks. As of now, I am using ISO15M for RS485 and SN65HVD235D for CAN and these transceivers are connecting to TMS320F283335 microcontroller…
Hello John,
Thank you very much for clear explanation. I am going ahead with SN65HVD235/232 transceivers and SN65HVD255D EVM.
Thanks for your support.
Regards,
Govind.
Hi Vivek
Thank you for the response, excuse me for make a lot of questions. But according to technical reference guide
The eZdsp F28335 has a 9 Pin female D-connector which brings out the CANA transmit and receive signals, This CAN interface uses the SN65HVD235…