Part Number: SN65HVD3086E Other Parts Discussed in Thread: SN65HVD1476 , SN65HVD34 Hi
C8051F384 with RS422 - 4 wire Full duplex communication ,
In the F/W Development
What is the Difference Half Duplex and Full Duplex in coding
Is standard keil Lib available…
Part Number: SN65HVD3086E Other Parts Discussed in Thread: LM22675 , LM25011 Dear Parker
We did further tests and would like to share our results. Request your advice.
1) During further tests, we find when the RS422 signals and DC_24V are separated and…
Part Number: SN65HVD3086E Project Code : Card Reader
Part Number : SN65HVD3086EDR Make : TI
Our customer require to run RS422 cable for 300 meter. On testing, we find the data communication stops at 48 meters.
Request advice what is the maximum distance…
Part Number: SN65HVD3086E Hello,
I have some questions for SN65HVD3086.
1)
The datasheet specifies input current of D and DE is -100 ~ 100uA.
According to Figure 21 on P13 of the datasheet, D had 50KOhm internal pull-up and DE had 50Kohm internal pull…
Part Number: SN65HVD3086E Hi, Customers are considering SN65HVD3086E for transmitter and receiver. Customers want to know the input current of 5V power supply. Transmitter side and receiver side termination resistance is 120Ω. If the input current depends…
Part Number: SN65HVD3086E Team,
The datasheet says “An internal Power-On Reset circuit keeps the outputs in a high-impedance state until the supply voltage has reached a level at which the device will reliably operate”. But I can’t find anywhere…
Part Number: SN65HVD3086E Other Parts Discussed in Thread: THVD1452 Hello to whom it may concern,
Our customer is considering to use the SN65HVD3086EDGS for the industrial HMI. In these condition is very hard. (Long Distance:50m, High noise) So, could you…
Part Number: SN65HVD3086E
Hi all, I will do like to replacement from MAXIM's device to SN65HVD3086. SN65HVD3086 has two Vcc ports. What do you have any concern if non connect one of them? MAXIM's device has one Vcc port, 13-pin is N.C. Regards, AC…
Part Number: SN65HVD3086E Other Parts Discussed in Thread: SN65HVD54 , THVD1550
Hi
We are looking for full-duplex RS-485 driver and receivers meeting following requirement.
Bit rate : 2.5Mbps
Length : 300m
Connection : 1 : 1
We are considering SN65HVD3086E…