Part Number: SN65HVD32 Tool/software: What is the exact source and sink current capacity for each of the Driver and Receiver pins of SN65HVD32 IC ?
Refer to the attached file taken from the datasheet.
RS485_sn65hvd32.pdf
Part Number: SN65HVD32 Hi Team,
We received PCN letter.
Then, Thermal Information of SN65HVD32DR is changed.
Could you please let us know why Thermal Information was changed?
<Rev L(Old)>
<Rev M(New)>
Regards,
Hide
Hi Hao,
Please find below RS422 transceiver protection circuit for our application:
Signalling speed requirement: 500Kbps
Surge waveform duration: 100usec
Residual transient current flowing into the IC: 1.25A
Note: As below circuit is already…
Part Number: SN65HVD32 Other Parts Discussed in Thread: SN65HVD35 , Hi support team,
Our customer is considering RS-485 communication with switching full - duplex or half - duplex. Therefore I am studying whether full-duplex RS-485 transceiver can be…
Part Number: SN65HVD32 Other Parts Discussed in Thread: SN65HVD30 Is SN65HVD32 available with EXTENDED PART (EP) which supports for defence and space applications??
Part Number: SN65HVD30 Other Parts Discussed in Thread: SN65HVD32 , Hi Team, Our customer would like to confirm if SN65HVD30 and SN65HVD32 can be interface to each other? They have two circuit cards. One with a 65HVD30 and one with 65HVDC32, so will the…
Part Number: SN65HVD32 HI,
we are using SN65HVD32DR (RS-485 full duplex - 8 pin ) for modbus commnication. This IC doesn't have RE/DE pin which is generally available with all rs485 IC for direction control. Further we are converting this full duplex…
Part Number: SN65HVD30-EP Other Parts Discussed in Thread: SN65HVD30 , SN65HVD35 , SN65HVD32 , SN65HVD33 Tool/software: Hi
I am doing a project that has one master and 60 slave. my MCU is STM32F103 and my data is in UART form. My connection mode is…
Part Number: SN65HVD35 Other Parts Discussed in Thread: SN65HVD32 Hi, I am looking for a TVS diode or chip varistor for bus protection of SN65HVD32. CDSOT23-SM712(Bourns) is used for protection devices in the data sheet.
Q1.I would like to use the following…