Part Number: SN65HVD63 We wish to use SN65HVD63 with a 8.704MHz crystal which has load capacitance of 40pF unlike the one on eval board which has a load capacitance of 12pF. Do you have any suggested capacitor value to be used for 40pF load capacitance…
Part Number: SN65HVD63 Hi team,
Can you please explain Figure 20?
tPHL and tPLH are specified from a point on the RXIN where the voltage is 0.5VL.
It doesn't make sense that 0.5VL is half the RXOUT voltage which is going to be ~2.5V for a 5V supply or…
Part Number: SN65HVD63 Hi INT team,
Can this part be adapted for a twisted pair operation?
From figure 24 in the datasheet there is a reference to twisted pair operation, could you explain this figure in more detail?
Is there app notes or more material…
Part Number: SN65HVD63 Hello
SN65HVD63 is Conforms to Proposed AISG V3.0 specification.
The emission spectrum is displayed in the datasheet up to 400Mhz.
but AISG v3.0 Request the Up to 12.75Ghz for emission spectrum.
Please let me know the emission…
Part Number: SN65HVD63 Other Parts Discussed in Thread: SN65HVD62 Hi, Team
My telecom customer plan to use SN65HVD63 in their smart antenna products.
1. They need to add lightning protection circuit on TXOUT/RXIN trace of SN65HVD63. There are several…
Part Number: SN65HVD62 Other Parts Discussed in Thread: SN65HVD63 ,
What are the ESR requirements for SN65HVD62 and SN65HVD63 external crystal oscillators? Spec not marked.
Part Number: SN65HVD1786 Other Parts Discussed in Thread: SN65HVD63 Hi Team,
My customer want to select a chip for change RS485 to PLC.
Only for DC not for AC
Power supply :5V or 3.3V
Carrier dc 12 or 24 VDC.
Or do we have solution to replace SSC P485…
Yukihiro,
Thank you for the details. I think you should be just fine to use these two parts together. You should not have a problem operating the SN65HVD63 at 10.5Mbps. I see that you have already implemented a fail-safe resistor network with R319…
Part Number: DS3695A Please forgive me if this question is silly. I'm having difficulty finding this information on the DS3695A's data sheet.
I need to know if this component needs external biasing on pins 6 and 7. Like what's pictured here:…
Rahul,
Ok, sounds good. Just to clarify, the first suggestion was to use both an RS-485 transceiver (to convert the differential signals to single-ended logic signals) and the SN65HVD63 (to translate those logic signals into an RF OOK signal).
Max