Part Number: SN65HVD70 Tool/software: Hello Team,
We are using SN65HVD70D in our application. Can you provide the characteristic impedance for RS422 differential signal lines?
Thank You.
Part Number: SN65HVD70 The terminal device is a slaver with SN65HVD7x,and the device runs at the status of low consumption of power,so that it can not support the IO "output current ,driver and receiver" mentioned in datasheet of SN65HVD7x。 …
Part Number: SN65HVD70 The data sheet shows it being available in the MSOP-10 3x3 mm package. I found it in the 10VSSOP which is 3x5 mm with the pin to pin length.
Part Number: SN65HVD70 Other Parts Discussed in Thread: SN65HVD76 , Hi Team,
One of our customers have noticed a minor discrepancy within the SN65HVD7x datasheet. Pages 4 and 5 of the datasheet provides the pin configuration for apparently the SN65HVD147x…
Part Number: SN65HVD70 Other Parts Discussed in Thread: RS485-FL-DPLX-EVM , Hi,
my customer would like to know how to connect RS485-FL-DPLX-EVM with AM335x UART.
Could you please tell us which pin on AM335x with DE and RE on SN65HVD70?
RS485-FL-DPLX…
Part Number: SN65HVD70 Hi Team,
Please help me answer the follow question, thank you so much.
SN65HVD70 IC is used in RS485 secification. The input A and the output Y are connected.
When the DE is set to "L" then the output is high impedance, the level…
Part Number: SN65HVD73 Other Parts Discussed in Thread: SN65HVD70 Hello,
we are using the SN65HVD73 transceiver with an UART input. The baudrate of the UART port is quite low (115200) and the cable length also short (<5m), so i thought we won't need any…
Part Number: SN65HVD70 Other Parts Discussed in Thread: SN65HVD37
I have a battery powered application in which need to give full duplex RS485.
1. System should be low power as battery powered
2. 3.3V vdd supply
3. Full duplex RS485
4. Length: 2 meters…