Part Number: SN65HVD71 Tool/software: SN65HVD71 datasheet is giving details of switching characteristics for 400 kbps. Please provide details of switching characteristics for 115.2 kbps.
Part Number: SN65HVD71 Hello E2E Experts,
The SN65HVD71 data sheet, section 7.8 and Fig. 20, list the maximum tpHL and tpLH as 110ns. A typical value is included, but not a minimum.
Is there a minimum value other than zero that can be used to determine…
Part Number: SN65HVD71 Tool/software: Hi, I have few questions design related
My Application would be using around 40mA meaning 40mA RS-485 IC would have to pass through it with around 1.8m Cable between Two devices Communication mode will be UART between…
Part Number: SN65HVD71 Tool/software: Hi, I am performing lightning transient surge testing on the 422 Transceiver and am seeing some results that do not make sense. First off, I have external TVS protection and series resistance as detailed in the datasheet…
Part Number: SN65HVD71 Could you please help us to see why the two screen prints are different? Is there any change, thank you In addition, when we test the output again, we found no output, help to see what is the reason, how to test the output
Part Number: SN65HVD71 Other Parts Discussed in Thread: SN65HVD72 , SN65HVD70 Tool/software: Hi,
I have designed a Full Duplex system using the SN65HVD71 transceiver. I would also like to use it in Half Duplex mode. Could you please advise me on the…
Part Number: SN65HVD71 Other Parts Discussed in Thread: SN65HVD1471 , SN65HVD1470 , SN65HVD70 , , SN65HVD73 , SN65HVD1473 , SN65HVD74 , SN65HVD1474 , SN65HVD1476 , SN65HVD76 , SN65HVD77 , SN65HVD1477 I can see that the ESD levels are higher and the thermal…
Part Number: SN65HVD71 Hello, I read the reference doc and I do not know how to configure the lines for the SN65HVD71DR. Here is why I have a conflict. I cant determine if the spec sheets say to do pullups or pulldowns on the R and D pins. It literally…
Part Number: SN65HVD71
Hi Team,
I have a question on SN65HVD7.
Since VID is -12V to 12V, the termination resistance is rated voltage higher than VID voltage. What is the rated voltage of the termination resistor of VOD. What voltage is VOD output…
Hi Michael,
It looks like there are several volts of "ringing" on the D input - do you know what could be causing this? I'm worried there may be some hardware issues related to that pin that prevent the signals from getting to the chip properly, since…