Part Number: SN65HVDA1050A-Q1 Other Parts Discussed in Thread: TCAN1051-Q1 Do we have P2P solution for this as we just need several Ku and my client is going to line down. THanks
Part Number: SN65HVDA1050A-Q1 Other Parts Discussed in Thread: SN65HVD251 , TCAN1051 Hello,
I'm redesigning my automotive scan tool and I want to use the SN65HVD251 instead of SN65HVDA1050AQDRQ1. The only relevant difference I found between them was the…
Part Number: SN65HVDA1050A-Q1 Other Parts Discussed in Thread: TPD2E007
Hello.
Please teach me the output impedance of the driver.
The reason why I want to know it is to check whether TPD2E007 with input capacitance of 15 pF can be used as a protection…
Part Number: SN65HVDA1050A-Q1 Hello.
SN65HVDA1050AQDRQ1 is directly connected to the TxD terminal of the MCU. The MCU is 3.3V. The output of the MCU is CMOS output. The TxD pin of SN65HVDA1050AQDRQ is internally pulled up to 5V. Therefore, when the output…
Hangjie,
The SN65HVD1050 was not designed to meet the same Automotive EMC standards that the HVDA551-Q1 was designed to pass. That includes integrated ESD protection, and that is likely what is showing here. The HVDA551-Q1 has better integrated ESD protection…
Other Parts Discussed in Thread: SN65HVD1050-Q1 , SN65HVD1050A-Q1 , SN65HVDA1050A-Q1 Hi Team,
My customer consider to use CAN tranceiver for automotive application.
I found following 3 devices.
1) SN65HVD1050-Q1
2) SN65HVD1050A-Q1
3) SN65HVDA1050A-Q1
…
Other Parts Discussed in Thread: SN65HVDA1050A-Q1 Hello, all
Now we have some inquiries regarding undervoltage threshold on SN65HVDA1050A-Q1 from our customer.
Please refer to the items below, and feedback us with your comment.
When referring RECOMMENDED…
Hello,
when viewing the CAN messages on our product (J1939 protocol) we discover that the last bit has a different voltage:
design:
CAN_Tx, CAN_Rx : to Piccolo DSP
CAN_High_inp, CAN_Low_inp : to connector of the product
setup:
product connected to…
If the SN65HVDA1050AQDRQ1 has no Vcc, no signal o nTXD, Vref=open, and a signal is a signal on CANH & CANL, what is the behavior of the part?
Can these conditions damage the part?
Other Parts Discussed in Thread: SN65HVDA1050A-Q1 Hi you.
Please give me a reply.
Has SN65HVDA1050A-Q1 followed up ISO10605 ?
As follows No1 and No2
My customer demand a ISO10605 Test-Level4.
This test-level is No1 and No2
・No1: Discharge for contact l…