Hi Tahir,
We do not have Raspberry Pi 3 schematic. Is it possible to send us as a reference? Then we can better understand your question regarding SN65HVS885.
Other Parts Discussed in Thread: SN65HVS885 Dear Sir
Customer would like to do short detect ,if input short to GND,we can indicate low or high to MCU
Could SN65HVS885 support this feature ,do you have recommend solution ??
Other Parts Discussed in Thread: SN65HVS885 Hello,
I am trying to create a footprint for the SN65HVS885 PWP HTSSOP package. I cannot find information regarding the size an position of the thermal pad. Datasheet and package drawing pdf refer to a separate…
Other Parts Discussed in Thread: SN65HVS885 We want to use the SN65HVS885 for 12V to 24V digital inputs. In our application we cannot make sure that there is always the 5V supply present when there is a voltage on the digital input pins.
What currents…
Other Parts Discussed in Thread: SN65HVS885 Hello Team,
We have connected 4 x SN65HVS885 in cascade mode. We read them successfully and correctly only when all of the RE (return) pins are connected to a common ground. Also, we needed to connect the…
Other Parts Discussed in Thread: SN65HVS885 Hello,
I can't understand the operation of SN65HVS885(Digital Input Serializer) after reading the TOPIC:[Cascading for High Channel Count Input Modules].Is it operates on SPI ??? Please help me.
Regards…
Other Parts Discussed in Thread: SN65HVS885 Hello,
I have a SPI bus on which are connected a bunch of SPI compatible components.
Each of these components are selected via a dedicated CS/.
I would like to add a SN65HVS885 Digital Input Serializer…
Hi,
according to http://www.ti.com/lit/ds/symlink/sn65hvs885.pdf Figure(18) an ISO7241 is used to isolate the SPI Pins. In Figure(19) a ISO724 2 is used because CE got grounded and HOT (Temp. warning Flag) is a new input.
Why CE is got pulled down…
Part Number: SN65HVS883 Other Parts Discussed in Thread: SN65HVS882 , SN65HVS885 Tool/software: Hello all,
I won’t have 24V to power the SN65HVS883. However, document "IIF-Training_Digital Input Serializers.pdf" indicates I can back-power the chip…