Ethan Sempsrott ,
Thank you for your recommendations. I have a couple more questions.
1) I could not get the 556 ohms and 135 ohms resistors (fail-safe biasing and termination resistors). Instead, 549 and 133 ohms resistors of 0.5 watts (0805 package)…
Part Number: SN65LBC173A Other Parts Discussed in Thread: SN65LBC180A
Hi Experts,
I am unable to find any information on the maximum and minimum storage temperature for SN65LBC173AD in its data sheet. Can you provide me with these figures?
I am asking…
Part Number: SN65LBC173A-EP Team,
I had a question about this RS-485 receiver. Does this part have Schmitt triggers on the inputs? I see the logic diagram with the Schmitt symbol, but no mention of it anywhere in the datasheet.
Also, I was wondering…
Part Number: SN65LBC173A Other Parts Discussed in Thread: TB5D2H The SN65LBC173A has internal pullup/pulldown resistors on both inputs.
From the functional block diagram, it looks like 100kΩ pullup, a series 18kΩ resistor, and then another few kΩ pullup…
Part Number: SN75115 Other Parts Discussed in Thread: SN75ALS193 , SN65LBC173A , If you had a choice between SN75115, SN75ALS193 or SN65LBC173A, which would you choose and why? (Assuming cost was not a factor)
Consider the application where the input differential…
Part Number: SN65LBC173A-EP Hi Team, I would like to get your input regarding the inquiry of the customer below: In the customer's design, he is driving IC's output low. The question is if the differential inputs' rising delay is a bit large(~15ns), will…
Hi Zoey,
The MAX device you reference is a 4T0R RS422 driver but AM26LS32A is our 0T4R RS422 receiver.
Did you mean the MAX33078 or MAX33079 (their 4x RS422 receivers)?
You can take a look at SN65LBC173A , this is a 4x RS422 receiver that can support the…
Part Number: SN65LBC173A Hi support team,
When differential input (VID) is "OPEN" under the condition of Enable G = X and Gn = L, will OUTPUT Y become 'H'? The condition of that combination is not described in the Function Table of SN65LBC173A…