Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: SN65LVCP114 Other Parts Discussed in Thread: DS100KR401 , DS100KR800 hi
The following is our application scenario. 10G data of SFP + is obtained through SN65LVCP114,Ethernet switching chips that pass through the backboard to the other single…
Part Number: SN65LVCP114 because the P/N of SN65LVCP114 can be swap,so,i want to know whether the P/N of Aout side and Bout side need to be swap at the same time if Cin was swap
if i configure the register through I2C interface?
thanks!
Part Number: SN65LVCP114 Other Parts Discussed in Thread: DS100KR401 Hi
Ethernet switching IC reaches SN65LVCP114 MUX IC through the backplane, the full high-speed signal protocol is 10GBASE-KR ,
After switching SN65LVCP114 MUXVIC switch, the signal protocol…
Part Number: SN65LVCP114 Hi TI,
In SN65LVCP114 EVM, used from 0.1uF 0201 capacitors for ac-coupling in RX/TX.
question 1: is there any recommendation for ac-coupling capacitors footprint in RX/TX? for example is it OK to use 0.1uF 0402 capacitor?
question2…
Part Number: SN65LVCP114 HI
We can see below comment in SN65LVCP114 DS
"Supports 10GBASE-KR Applications With Ability to Transparency for Link Training"
Customer is using SN65LVCP114 for KR mux so need to set the 10GBASE-KR with Ability to t…
Part Number: SN65LVCP114 If I understand correctly, the SN65LVCP114 can be put in diagnostic mode and split a 6Gbps signal. Just to make sure I am clear, I need to split the signal (one input, two simultaneous outputs) and not simply mux the signal. Are…
Part Number: SN65LVCP114 1、what is the I2C_SEL pin internal circuit structure? when use GPIO mode ,if can be floating ?
2、When use GPIO mode ,how to deal with the I2C_SCL/I2C_SDA ,if can be floating?
Thank you !
Part Number: SN65LVCP114 Can unused high speed inputs be left floating, or should they be biased? Design using 3 of the 4 inputs.
Blog note "Trouble passing 12G SDI" says inputs are biased to VCC-0.3 nominally.