Part Number: SN65LVCP114 SN651VCP114 hardware design, I want to use GPIO mode simultaneously compatible with I2C mode.
Our signal is 10G-KR.EQX1 and EQX0 how many db we choose? LOOPBACK enabled or disabled? /PWD high? enables the AGC loop? VOD_A hig…
Part Number: DS100KR401 Other Parts Discussed in Thread: SN65LVCP114 , , DS125BR820 , DS125BR401A , DS125BR401 I have a media converter design that converts between 10G-KR and 10G-SR (copper to fiber).
I was having issues getting the 10G-KR side to link/pass…
Other Parts Discussed in Thread: SN65LVCP114 Hi,
Just for test, I want to disable all functions such as EQ, and use SN65LVCP114 as switch.
at this test, the only thing I need is just select lanes, and do not disturbed by other functions.
If this possible…
HI Michael,
We ran into this problem right now. We have design that use this SN65LVCP114 back to back and to SFP+ on C port. We shall the eye got distorted. The length from this device is 3" to the SFP and about 2.5" between the SN65LVCP114.…
Other Parts Discussed in Thread: SN65LVCP114 This is an urgent critical request. We are seeing quite a bit of jitter when we are going the SN65LVCP114 redriver chip.
Our application on this TI-MUX chip (SN65LVCP114) is passing SFP+ traffic from A to B…
Other Parts Discussed in Thread: SN65LVCP114 Hello Team,
Please allow me to confirm the internal pull-up / pull-down resistor value of SN65LVCP114. There are difference between the datasheet and user guide. I believe the datasheet value of 48k is true…
Other Parts Discussed in Thread: SN65LVCP114 When designing with the SN65LVCP114 using an older datasheet, there was no mention of needing 5k pullup/pulldown resistors on config pins, so the pins were left floating on a customer design. Now, the datasheet…
Other Parts Discussed in Thread: SN65LVCP114 Hello,
I am planning on using an SN65LVCP114 for an RXAUI application and am curious about the expected power dissipation. In this application only two of the the three ports will be used and the maximum data…
Other Parts Discussed in Thread: SN65LVCP1414 , SN65LVCP1412 , SN65LVCP114 Hello,
In my application, only two of the three available ports will be used. Is there a recommended strategy to setting the unused ports IO? (e.g. ground inputs, leave outputs…