Part Number: SN65LVCP22 Other Parts Discussed in Thread: TS5A23157 , TMUX582F-SEP , SN54HC157-SP , SN54HC138-SP , SN54HC08-SP , SN54HC32-SP Tool/software: Hello Team, Is it possible to use SN65LVCP22 as UART (TX and RX only) MUX 2 to 1?
Thanks, Moral.
Part Number: SN65LVCP22 Tool/software: Hi Team, I would Like to use SN65LVCP22 as a MUX, Should I leave the the unused pins floating to tie it to GND? Please confirm the following connections: OUT1+ -> GND OUT1- -> GND EN1 -> GND SEL1 -> GND EN0…
Part Number: SN65LVCP22 Hi,
Let me ask you some basic questions as below.
Q1) unusued IN+/IN- pins
Will you tell me how to handle these pins in case unusing?
Is it possible to leave "open"?
Q2) EN0/EN1
In case of using these pins with "H" fixed…
Part Number: SN65LVCP22 Hi, Good day. Our customer would like to know what to do with the enable pin.. A re the enable pins active high? ...can they be tied high with a resistor? Looking forward to your feedback. Thank you, Cedrick
Part Number: SN65LVCP22 Hello. Let me ask you some questions about the SN65LVCP22.
1. Does SN65LVCP22 have a built-in FAIL SAFE function? Looking at the circuit principle diagram, it does not seem to have the FAIL SAFE function.
2. I think you will add…
Part Number: DS38EP100 Tool/software: Are there any replacement or suitable evaluation kits that perform the same function as these two TI part numbers:
DS38EP100-EVK
SN65LVCP22-23EVM
I see that the two component-level parts are still manufactured and…
Hi Nasar,
Thank you for your support, please clarify below questions.
1. If i use SN65LVCP22 is 1x2 splitter, whether SN65LVCP22 is drive as repeater passive or Read and Drive?
2. How u say iMX6 LVDS support up 1Gbps? If iMX6 is 1Gbps then i am good to…
Thanks Josh, SN65LVCP22 will support 4K and 1080p Video, I am using conversion after lvds spillter, to connect to monitor, DS25CP152TSQ/NOPB is better part compare to SN65LVCP22? Because i little bit varied about transmitted speed.