Part Number: SN65LVCP402 Hi Team,
Could you provide an IBIS model for SN65LVCP402?
I found this E2E website: https://e2e.ti.com/support/interface-group/interface/f/interface-forum/596458/sn65lvcp402-request-for-ibis-model
Then I reached to …
Part Number: SN65LVCP402 Other Parts Discussed in Thread: LMKDB1202 Is the SN65LVCP402 suitable for PCIe Gen5 clock buffer/MUX? If not, do you have any other recommendations?
Part Number: SN65LVCP402 Other Parts Discussed in Thread: DS25CP102 Hi,
I found a thread saying that there is no IBIS model for SN65LVCP402.
I was wondering if you could tell me the replacements that has similar features and IBIS model to SN65LVCP402…
Part Number: SN65LVCP402 Hi,
I have any question.
1. When VBB Pin is left open, is it correct to recognize that the voltage of VBB Pin will be 1.6V?
2. When our customer measured the voltage of VBB Pin that left open, VBB = 0V.
Do you know the…
Part Number: SN65LVCP402
Hi,
Our customers are thinking of a design like the one shown below.
Is it possible to cascade connection from SN65LVCP402RGE (a) on substrate (a) to SN65LVCP402RGE (b) on substrate (b)?
Best Regards,
Nishie
Part Number: SN65LVCP402
Hi,
Out customers are thinking of a design like the one shown below.
Is it possible to input to CML after AC coupling 1.5V PCML?
Also, is it possible to output to 1.5V PCML after AC coupling VML?
Best Regards,
…
Part Number: SN65LVCP402 Hi,
Our customers are thinking of a design like the one shown below.
Is it okay if the value of the capacitor for AC Coupling is 0.1uF?
Best Regards,
Nishie
Eli,
I am not sure what features are needed for the customers application but they may want to consider a device like SN65LVCP402 that can be used as a two channel repeater with RX EQ and TX pre-emph/de-emph as one possible option. Note that SN65LVCP402…