Part Number: SN65LVDS1 Hi Team,
Can you please check and advise with following request:
"
I need SN65LVDS1DBV junction-to-board thermal resistance value. There is not enough information available in the datasheet. If you can find this information…
Part Number: SN65LVDS1 Hi,
The DC characteristics of driver mention IIH and IIL currents, need clarity on whether this current is drawn even when Vcc = 0, or it is only applicable when device is operating between 2.4V to 3.6V.
Similarly, IIL current…
Hello Yaser,
Thank you for your complete answer and now it is clearest for my design.
Your explanations contributes to validate my hypotheses.
Best Regards,
Julien
Part Number: SN65LVDS1 Other Parts Discussed in Thread: SN65LVDT2 Hi Guys
Customer want to use our SN65LVDT2 device, but we find that the rise time is 0.6ns(typical). it is a little bit longer. Do we have higher performance device? around 0.35ns rise…
Hello Shanu,
Please see the answers below.
1) Yes, you can connect the AVC4T245 to the LVDSS1.
2) Yes, you can connect the LVDS2 to the AVC4T245
3) there is not problem connecting a CMOS output to a TTL input.
4) There is not possible to have…
Part Number: SN65LVDS1 Other Parts Discussed in Thread: SN65LVDS4 As in the topic - do we have a differential line driver suitable for 1.8V supply?
We have a receiver with 1.8V support (SN65LVDS4), but I cannot find a suitable driver.
Thanks
Part Number: SN65LVDS1 Other Parts Discussed in Thread: DS90LV017A , SN65LVDS2 , DS90LV018A , We have 2 circuit boards that need to communicate over an external LVDS cabled interface. The interface is a basically a master/slave SPI bus using the LVDS…