Part Number: SN65LVDS100 Hi team,
Customer feedback the LVDS application circuit exist the problem of resistance breaking and lead to can’t output PG signal.
Details are in the attachment, can you give some suggestions about it?
Attached information…
Part Number: SN65LVDS100 Dear Technical Support Team,
SN65LVDS100DGKR has a symptom where the LVDS output does not come out when the power is turned on/off.
connection FPGA ⇒ SN65LVDS100DGKR ⇒ Cable ⇒ Receiver (not TI)
Are there any similar defects…
Part Number: SN65LVDS100 Other Parts Discussed in Thread: CDCLVD2102 , Hi,
I want to use this device for buffering a clock toward FPGA that have also phase noise input requirements (dbc values at several frequencies).
do you have a phase noise graph…
Part Number: SN65LVDS100 Other Parts Discussed in Thread: DS90LV017A Hi,
I have the device, P/N: SN65LVDS100DGK.
Can I input it a 10MHz clock, LVCMOS format, and output the LVDS differential output?
How Can I connect the above LVCMOS to that device…
Part Number: SN65LVDS100 Other Parts Discussed in Thread: DS15BR401 hi,
Customer requires a BUFFER without termination resistor.
The input to the buffer is DS15BR401TSQ/NOPB(TI) output.
The SN65LVDS100 appears meet the above requirement--there are…
Part Number: SN65LVDS100 Hello,
I need to implement AC coupling on the inputs of the SN65LVDS100 LVDS repeater (based on figure 50 in its datasheet). If the SN65LVDS100 is off (as the rest of the board) and there is activity on the LVDS lines, it…
Part Number: SN65LVDS100 In the Datasheet, figure 48 shows a Vcc/2 bias for a cmos input.
Will this also work for the SN65LVDT device with the built in termination?
The absolute range Vid says 1V. Does this Vid of 1V apply to both devices with or…
Part Number: SN65LVDS100 Hi,
for specific applications, we have to eliminate any floating metal
I have very few PCB surface and I need to optimize qty of components
My goal was to connect the NC pin (pin 1) to VCC pin 8 (or GND or VBB)
can you…
Part Number: SN65LVDS100 Other Parts Discussed in Thread: DS90LV047A , , SN65LVDS31 , DS90LV031A Hi
we have a bus of 10 signals that we have to translate from CMOS_1V8 to LVDS.
we understand that we need to bias the "-" input to 0.9V by using resistor…