Part Number: SN65LVDS179 Hi,
I'm trying to download the SN65LVDS179 IBIS model but on the product page the links go to 404 error pages.
Can the IBIS model be provided or restored to the product page?
Part Number: SN65LVDS179 Hi TI team,
We are using "SN65LVDS179DR" as LVDS transceiver/receiver for delta sigma lines for voltage measurement. We are using a 4.5meter high speed cable for transferring the measurement between two PCBs. The measurement…
Part Number: SN65LVDS179 Tool/software:
hello Team,
my output is LVDS, i need to convert this LVDS output to UART so can i give LVDS transmitter
output to one SN65LVDS179 IC
Y (pin 5) to another SN65LVDS179 IC Y (pin 5),
Z (pin 6) to another…
Part Number: SN65LVDS179
Tool/software:
Hello,
My customer noted that the test circuit figure, figure 12, mentions a 1ns rise and fall times and is asking if the input to the driver (D) or differential input (A & B) have any rise and fall time requirements…
Part Number: SN65LVDS179 hi,
my customer use SN65LVDS179 to implement the communication between LVDS and LVPECL (from SFP optical module) . its schematic and SFP's LVPECL output parameters are included in the attach. Pls kindly help check if the schematic…
Part Number: SN65LVDS179-EP Other Parts Discussed in Thread: SN65LVDS179 Hello team,
What would be the data speed for SN65LVDS179-EP, if all buffers are active?
On the datasheet for SN65LVDS179 (Non EP version), it says only 150Mbps when all buffers…