The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.
Part Number: SN65LVDS180 Other Parts Discussed in Thread: SN65LVDS31-EP , SN65LVDS33-EP Tool/software: Hello. I need a LVDS transceiver that is rated to work at -55C. The SN65LVDS179MDGKREP rated to work at -55C is on the datasheet and is available in distribution…
Part Number: SN65LVDS180 In the event that the device is unpowered, can the LVDS receiver inputs be driven without risk of part damage or stress? From the datasheet, I’m inclined to think this is the case, but I wanted to double check.
Part Number: SN65LVDS180 Im trying to design with the following lvds transceiver: SN65LVDS180PW and was concerned about the state of the tx output when its disabled. The data sheet only states that the lvds output is 'OFF'. Does this mean its high-Z? Thank…
Part Number: SN65LVDS180 Other Parts Discussed in Thread: SN65LVDM176 We are using the SN65LVDS180 device to drive a differential signal across a cable which is 50 feet long. The same device (SN65LVDS180) is used on both ends of the cable as the driver…
Part Number: SN65LVDS180-Q1 Hi Team, Our customer has a question concerning the IOS parameter of SN65LVDS180-Q1. Does the device have a protection circuitry that allows its differential outputs to be shorted indefinitely? If not, how long can the outputs…
Hi Zou,
The DS90LV012A does not have the ability to tri-state its output. We do have some multichannel LVDS receivers such as the SN65LVDS390 with output enables to tri-state the output. We also have LVDS transceivers with driver/receiver enables such…
Part Number: SN65LVDS180 I'm trying to identify the difference between the SN65LVDS180PWRQ1 and SN65LVDS180PWRG4Q1 parts listed on the SN65LVDS180 datasheet. The lead finish is identical in the datasheet as Cu NiPdAu. There are no identifiable differences…
Part Number: SN65LVDS180 We have a setup where there’s a chance this part could be powered off while the FPGA driving it could be powered on. Is there any information on if this will cause the board VCC plane to be powered up in this case? We have the…