Part Number: SN65LVDS2 Tool/software: Hi team,
My customer designs this device(SN65LVDS2DBVR) in their system.
And they tried to do open-Circuit Fail-Safe test. This Receiver's output become high when there is no signal in Input side.
So do we have…
Part Number: SN65LVDS2 Hi all,
i'm working on API 2.0.
When i try to make an order I always receive error 500, I use this partnumber: www.ti.com/.../SN65LVDS2DBVR
this is the json request (i use only required fields)
{ "checkoutProfileId": "XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX…
Hi Josh, I did..
From Customer Support:
Thank you for contacting TI Customer Support and choosing TI Product for your project.
Our experts would like to engage with you regarding this inquiry in our e2e forum. TI E2E design support forums are an engineer…
Part Number: SN65LVDS2 Hello Team.
Can you share with us the theta JB and theta JC for the SN65LVDT2DBVR? The datasheet only shows theta JA.
Regards, Renan
Part Number: SN65LVDS2 Hello Team,
under which conditions min and max values below are tested?
In your datasheet a min and max value for the propagation delay is given. For example, min-value is 1.4 ns and max-value is 3.6 ns. Where does the difference…
Part Number: SN65LVDS2 What are the thermal resistances of the for the SN65LVDS2D from junction to bottom case (Theta_JC) in C/W ( 8-SOIC package) and the junction to top of the case (Theta_JT) in C/W?
The SN65ELT21 is a PECL-to-TTL translator, but only for 5 V.
The application report DC-Coupling Between Differential LVPECL, LVDS, HSTL, and CM shows in figure 5 how to terminate LVPECL for an LVDS receiver (e.g., SN65LVDS2).
Part Number: SN75LVDS387 Other Parts Discussed in Thread: CDCE6214-Q1EVM , SN65LVDS2 , SN65LVDS4 , DS90LVRA2 , SN75LVDS386 Tool/software: Hi team,
Is the related post/question still true? ( https://e2e.ti.com/support/interface-group/interface/f/interface-forum…
Part Number: SN65LVDS2 A/B pins measured a low +0.268V, high +0.668V diff clock, but no output on R pin
i think Vid -0.4V/+0.4V and Vcm 0.468V are both compatible with spec requirement
A/B pin are terminated with an external 100Ohm.
then what's the issue…
Part Number: SN65LVDS2 Other Parts Discussed in Thread: SN65LVDS1 Hi,
In the datasheet under the switching characteristics table, you list out the test conditions for your AC measurements. These conditions are 100ohm load with 10pF cap, and list the 10…