Part Number: SN65LVDS2 Team,
is it possible to estimate, whether when operating SN65LVDS2 (SOT-23-5 package) at PCB temperatures of 85°C or 90°C, the lifetime of the device can be impacted (shortened)?
Our PCB is completely embedded in a plastic protective…
Part Number: SN65LVDS2 Hi Team
Would you advise about below two inquiry?
① About A / B pin If the input CLK is LVDS, is there a problem with direct connection? (CLK output IC - AC coupling capacitor etc between the IC is unnecessary? Just to be sure…
Hi Andrew,
Our prior experience informed us that PSPICE doesn't support IBIS, and that the translator somewhat supports just input buffers.
Doing a quick search, I see that version 16.6 claims to support IBIS, including VT waveforms. I don't have…
Part Number: SN65LVDS1 Other Parts Discussed in Thread: SN65LVDS2 ,
Dear Technical Support Team,
I have two questions for SN65LVDS1 and SN65LVDS2.
1.)Could you tell me "Differential Part to Part Skew" ?
2.)Could you tell me the min value of Propagation…
Part Number: SN65LVDS1 Other Parts Discussed in Thread: DS90LV017A , SN65LVDS2 , DS90LV018A , We have 2 circuit boards that need to communicate over an external LVDS cabled interface. The interface is a basically a master/slave SPI bus using the LVDS…
Hello Team,
the text below the package pictures on the first page of the data sheet tells "110 Ohm Resistor for LVDT only".
Does this mean: an external resisitor is required for LVDT or the resistor is integrated?
According the AVAILABLE OPTIONS…
Hi Mohammed,
Can we close this post out or will you be following up with more questions about the SN65LVDS1 and SN65LVDS2?
Regards,
Michael Peffers
High Speed Interface Applications