Part Number: SN65LVDS302 Tool/software: Hi,
I am planning to use SN65LVDS302 in my design. I was not able to located if RGB lines are push pull or open drain.
Request you to clairify.
Regards,
Anurag
Part Number: SN65LVDS302 in previous design we used SN65LVDS308ZQCR
right now, it is discontinued.
can i use SN65LVDS302ZXHR with same configuration
can you please conform if there are any software changes are required if i use SN65LVDS302ZXHR?
SN65LVDS302ZXHR…
Part Number: SN65LVDS302 Other Parts Discussed in Thread: DS90CF364A Hi,
Can SN65LVDS302 transmit 16-bit data of YCbCr if using the data lanes of D0 and D1(D2 is not be used) with 3-channel mode which is mentioned on page 29 of SN65LVDS302 data sheet…
Hello Ajay,
we do not have any single chip solution which can converts sub-LVDS to MIPI CSI-2. However we do have this device which receives up to 3 sub-LVDS data pairs and one CLK pair, and outputs RGB parallel data (SN65LVDS302)
Part Number: SN65LVDS311 Other Parts Discussed in Thread: SN65LVDS301 , SN65LVDS302 ,
Hi,
Our customer has used a combination of SN65LVDS301 and SN65LVDS302 in the past.
Now, he is trying to replace SN65LVDS301 with SN65LVDS311 in the new design.
So, could…
Part Number: SN65LVDS302 Hi, Could you tell me about tR/F spec? The following contents are described in the data sheet.
However,My customer wants to know the capability value.
Could you please let us know the ability distribution of tR/F specification for…
Other Parts Discussed in Thread: SN65LVDS302 Hello,
Our customer uses the SN65LVDS302, with 3ch mode.
The customer uses a CLK as
fCLK=54MHz
fMOD=24.816kHz
modulation amount +1.0% ,-1.0%
Can the SN65LVDS302 receive the above signal for PCLK?
Regards,
Naoki…
Other Parts Discussed in Thread: SN65LVDS302 Hello,
My customer uses the SN65LVDS302, wants to know the storage temperature range.
It is mentioned the operating temperature range '-40 to +85 degree ' on the datasheet.
But there is no information…
Other Parts Discussed in Thread: SN65LVDS302 Hello,
My customer uses the SN65LVDS302.
He wants to know the junction temperature by observe the case temperature.
So, could you give me the junction-to-case thermal resistance?
Regards,
Naoki Aoyama