Part Number: SN65LVDS315 Hello Team,
I am looking for a RGB888-to-MIPI bridge and I found the SN65LVDS315. I am not sure if this is the best fit, do we have other devices and do we have something newer in our portfolio?
thank you.
Kind regards…
Tool/software: Hi Expert,
My customer have below demands, could you please help to check if we have related solution, which should be Automotive Grade devices, thanks in advance!
1 、 4 channels CVBS -> MIPI 2 、 HDMI -> CVBS 3 、 MIPI -> CVBS 4 、 OPEN…
Part Number: SN65LVDS315 Tool/software: Simple explanation:
I have a 258.3 MHz fiber optic signal. This signal is 8b/10b encoding of RAW8 video, in a 1640 by 525 format. It is running at 60 Hz field rate interlaced, so 30 Hz frame rate. The video uses…
Part Number: SN65LVDS315 Hi TI experts,
Now customer want to select a bridge IC which is used to transfer RGB565/666/888 to MIPI.
The interface of SOC is RGB and the interface of screen is MIPI.
I just found a IC which is SN65LVDS315., It can only…
Part Number: SN65LVDS315 Other Parts Discussed in Thread: DS90UB934-Q1 , DS90UB935-Q1 Hi Team,
Can I get an IC that converters mipi_csi to rgb?
The opposite direction of sn65lvds315.
Thanks in advance.
With regards,
Jayashree.
Part Number: SN65LVDS315 Other Parts Discussed in Thread: DS90UB936-Q1 Hello,
Could this device SN65LVDS315 support 8/10bit DVP signal input, MIPI DPHY output?
If not, could you pls recommend suitable device?
thanks.
Part Number: SN65LVDS315 Dear team,
I would like to know which solution is suitable for customer requirement.
< Customer requirement>
- input : MIPI CSI format
- output : parallel 10 bit pixel data
Is there any solution to fit customer application…